cancel
Showing results for 
Search instead for 
Did you mean: 

how much KOhm is the pullup or pulldown resistor of GPIO pins ?

mehmet.karakaya
Associate III
Posted on December 02, 2012 at 18:26

typedef enum

 

{.......

 

 GPIO_Mode_IPD = 0x28,

 

  GPIO_Mode_IPU = 0x48,

 

......

 

  }GPIOMode_TypeDef;

hello forum,

I have two questions ;

1) do the above settings make the GPIO pin Input ?

2) if I adjust the GPIO pins according to above settings

how much KOhm is the pullup or pulldown resistor of GPIO pins ?

thanks

#gpio-pullup-pulldown
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on December 02, 2012 at 18:48

IPU Stands for Input Pulled Up,so yes an input.

The Pull Up/Down value is in the manual, nominally 40K (30-50 across process corners). See ''I/O static characteristics''

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..