How doi use the stm32f207vgt6 HAL Library to write and read the EEPROM using I2C.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-12 11:30 PM
void MX_I2C1_Init(void)
{ HAL_I2C_MspInit(&hi2c1);hi2c1.Instance = I2C1;
hi2c1.Init.ClockSpeed = 100000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; hi2c1.Mode = HAL_I2C_MODE_MASTER; if (HAL_I2C_Init(&hi2c1) != HAL_OK) { xprintf_temp('I2c1 Init error'); Error_Handler(); }/* Enable the selected I2C peripheral */
I2C1->CR1 |= I2C_CR1_PE;}void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
{GPIO_InitTypeDef GPIO_InitStruct;
if(i2cHandle->Instance==I2C1) { /* USER CODE BEGIN I2C1_MspInit 0 *//* USER CODE END I2C1_MspInit 0 */
/**I2C1 GPIO Configuration PB6 ------> I2C1_SCL PB7 ------> I2C1_SDA */ GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_I2C1; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* Peripheral clock enable */
__HAL_RCC_I2C1_CLK_ENABLE(); /* USER CODE BEGIN I2C1_MspInit 1 *//* USER CODE END I2C1_MspInit 1 */
}}char temp[15],val = 0;
val = HAL_I2C_Master_Transmit(&hi2c1,0x18,'EEPROM TEST',15,100000);HAL_I2C_Master_Transmit it retuns 1(i.e HAL_ERROR)
val = HAL_I2C_Master_Receive(&hi2c1,0x18,temp,15,100000);
HAL_I2C_Master_Receive it retuns 1(i.e
HAL_ERROR)
while am receiving the data (i.e temp data) . am not getting original data.
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-13 5:34 AM
on the premise that your device's address in the data sheet is 0x18
uint8_t d[3];
d[0] = (reg_addr >> 8) & 0xFF; // high byte of 16-bit register address
d[1] = (reg_addr) & 0xFF; // low byte of 16-bit register address d[2] = value; // what value are we writing to the registerwhile (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x18<<1), 3, 100) != HAL_OK) {} //wait until the device is ready
if (HAL_I2C_Master_Transmit(&hi2c1, // i2c handle
(uint16_t)(0x18<<1), // i2c address, left aligned (uint8_t *)d, // pointer to the buffer containing the data sizeof(d), // how many bytes are we transmitting 1000) // timeout value != HAL_OK) // result code { printf('master transmit failed\r\n'); Error_Handler();}
read is the same way except you do a transmit then a receive
uint8_t value;
while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x18<<1), 3, 100) != HAL_OK) {} //wait until the device is ready
while (HAL_I2C_Master_Receive(&hi2c1, // i2c handle
(uint16_t)(0x18<<1), // i2c address, left aligned (uint8_t *)&value, // pointer to address of where to store received data 1, // expecting one byte to be returned 100) // timeout != HAL_OK) // result code{
printf('master receive failed\r\n'); Error_Handler();}
to read and write registers, its often more handy to use Mem_Read and Mem_Write
while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(dev_addr<<1), 3, 100) != HAL_OK) { }
status = HAL_I2C_Mem_Read(&hi2c1, // i2c handle
(uint8_t)(dev_addr<<1), // i2c address, left aligned (uint8_t)reg_addr, // register address I2C_MEMADD_SIZE_16BIT, // 16bit register addresses (uint8_t*)(&array), // write returned data to this variable cnt, // how many bytes to expect returned 100); // timeoutif (status != HAL_OK)
{Error_Handler();
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 4:36 AM
this code struct at
while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x18<<1), 3, 100) != HAL_OK) {} //wait until the device is ready
and what will be the value of
reg_addr,value and dev_addr .
HAL_I2C_Master_Transmit(&hi2c1,0x18<<1,'EEPROM TEST',15,100000);
HAL_I2C_Master_Receive(&hi2c1,0x18<<1,temp,15,100000);
in this am getting the size of the buffer, but didn't get the correct data.
am using EEPROM 24C256 in that SCL and SDA is connected to External pullup 4K7.
when am used standard peripheral library its working good.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 5:16 AM
reg_addr is the register address you wish to access in the eeprom
dev_addr is the i2c address of the device
the HAL wants a pointer to a buffer so try (uint8_t *)&temp instead of just temp
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 6:11 AM
HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x18<<1), 3, 100) returns
HAL_ERROR.
Still i didn't get any idea why my code is not working..
please can any one healp me..
thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 6:45 AM
it looks like you've modified initialization code that the cubemx application generated. try the initialization code it generates without modifying it
also, what does HAL_I2C_GetState(&hi2c1) return when you call it after MX_HAL_I2C_Init()
its either your initialization code or your wiring, at this point.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-15 2:04 AM
my EEPROM DevAddress is 0xA0
the MSB bit of
DevAddress is 0 for writing and 1 for readeing.
val = HAL_I2C_GetState (&hi2c1);
print('HAL_I2C_GetState = %x', val);val = HAL_I2C_Master_Transmit (&hi2c1, (uint16_t) 0xA0, '
EEPROM
', 10, 10000);val = HAL_I2C_Master_Receive (&hi2c1, (uint16_t) 0xA1,&temp, 10, 10000);
am getting:
HAL_I2C_GetState = 20 //
0x20 i.e
HAL_I2C_STATE_READY = 0x20U, /*!< Peripheral Initialized and ready for use */
HAL_I2C_Master_Transmit error = 0HAL_I2C_Master_Receive error = 0HAL_I2C_Master_Receive data = ÿÿÿÿÿÿÿÿÿÿ