cancel
Showing results for 
Search instead for 
Did you mean: 

How do I get the IP address using dns_gethostbyname()?

snaghyun choi
Associate III

cpu : stm32f4

I want to get the IP address using dns_gethostbyname. However, I can not get the IP address

How do I get the IP address ?

( I set the DNS service using stm32cubeMX.)

==================================

void main(void)

{

   int test=dns_gethostbyname("www.freertos.com",&resolved,dns_found,NULL);

}

void dns_found(const char *name, ip_addr_t *ipaddr, void *arg)

{

 uint8_t ip[4];

 ip_addr_t result = *ipaddr;

 ip[0] = result.addr>>24;

 ip[1] = result.addr>>16;

 ip[2] = result.addr>>8;

 ip[3] = result.addr;

 printf("%d.%d.%d.%d\n",ip[3], ip[2], ip[1], ip[0]);

}

=================================================

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0