2018-08-14 4:33 AM
I want to do a C Project in Eclipse using the STDPeriph. But when selecting the STM32F407G-DISC1, there is no firmware defined for this target.
2018-08-14 4:57 AM
Don't things like Atollic or SW4 use "Eclipse" ? Can you not port or replicate the "Workspaces" to create your own project?
The SPL has relatively simple requirements, you'd want to set up the Include Paths so the library .H files can be found, and then pull all the used library .C files into your project, and set the command line compiler defines with USE_STDPERIPH_DRIVER
See
STM32F4xx_DSP_StdPeriph_Lib_V1.8.0\Project\STM32F4xx_StdPeriph_Templates\SW4STM32\STM32F40_41xxx\.cproject
STM32F4-Discovery_FW_V1.1.0\Project\Peripheral_Examples\ADC3_DMA\TrueSTUDIO\ADC3_DMA\.cproject