cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am trying to connect ESP8266 module to STM32F429ZI so I am wondering if (and which) transmit pins of UART transmit max voltage of 3.3V (not 5V)? Thanks in advance!

MCulj.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

All STM32F4 pins transmit at 3.3V (or whatever your VDD is). None of them transmit at 5V, although most of them are 5V tolerant for input signals.

If you feel a post has answered your question, please click "Accept as Solution".