cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I'm using STM32L151RET6 now. Can STM32L152RET6 be an alternative, or will I need SW modification? Thank you!

DLev.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @DLev.1​ and welcome to the Community :)

Yes, possible to use STM32L152RET6 as it's full compatible with STM32L151RET6.

If your question is answered, please close this topic by choosing Select as Best.

This will help other community members finding that answer faster.;)

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
Imen.D
ST Employee

Hello @DLev.1​ and welcome to the Community :)

Yes, possible to use STM32L152RET6 as it's full compatible with STM32L151RET6.

If your question is answered, please close this topic by choosing Select as Best.

This will help other community members finding that answer faster.;)

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thank you, Imen!

diegofontanabr
Associate II

if the two are absolute the same, why do you have both? i dont belive that, there must have some differente.... to star with, in the product selector it says 151 have dual boot and 152 not.