cancel
Showing results for 
Search instead for 
Did you mean: 

hello, I am working in a project with STM32f100 and I want to set this MCU as a slave using I2C interface. the master should be raspberry PI so I need the address of STM32.

Mohammed_BEN
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bubbles
ST Employee

You need to configure the address in the I2C register, I2C_OAR1 or I2C_OAR2. More info in RM0008.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Bubbles
ST Employee

You need to configure the address in the I2C register, I2C_OAR1 or I2C_OAR2. More info in RM0008.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Mohammed_BEN
Associate II

I have configured a slave address in CUBEMx, but when I open my raspberry and try to detect I2C signal, I can't see any thing. any suggestions?

what code is loaded to the STM32? Try some example from the Cube Introduction package. There are several examples of I2C communication.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Mohammed_BEN
Associate II

ok thank you, now is working I can get some a result