Skip to main content
mike louaillier
Associate III
July 15, 2017
Solved

Hello are there any specs from ST on reflow temperatures for a TSSOP 20 chip?

  • July 15, 2017
  • 1 reply
  • 2446 views
Posted on July 15, 2017 at 21:58

can't find one word on their site about temperatures for soldering.

    This topic has been closed for replies.
    Best answer by Tesla DeLorean
    Posted on July 15, 2017 at 22:22

    Definitely an area where the documentation you'd expect to find such detail has it missing.

    Google AN2639 Soldering Recommendations, couldn't find a linkable copy on ST's site. Have attached

    ________________

    Attachments :

    en.CD00173820.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyZG&d=%2Fa%2F0X0000000b9Z%2FBgvxm1e710Ve1Nedl369SD8V4mVqOZqq.YxMmDzMZV4&asPdf=false

    1 reply

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    July 15, 2017
    Posted on July 15, 2017 at 22:22

    Definitely an area where the documentation you'd expect to find such detail has it missing.

    Google AN2639 Soldering Recommendations, couldn't find a linkable copy on ST's site. Have attached

    ________________

    Attachments :

    en.CD00173820.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyZG&d=%2Fa%2F0X0000000b9Z%2FBgvxm1e710Ve1Nedl369SD8V4mVqOZqq.YxMmDzMZV4&asPdf=false
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mike louaillier
    Associate III
    July 15, 2017
    Posted on July 15, 2017 at 23:01

    thanx Clive One, yes and they don't have any references to AN2639. and no hope searching it out around here, either. maybe if i put in a few keywords it might help.

    reflow temperature profile hot air soldering specs specifications method limits heat

    AN2639 Soldering recommendations and package information for Lead-free ECOPACK microcontrollers

    T J
    Senior III
    July 17, 2017
    Posted on July 17, 2017 at 01:12

    Starting out, I wasn't sure what temperature to use;

    almost 10 years ago, I built a toaster oven to re-flow my PCBs.

    but I wasn't sure what temperature to use.

    Some datasheets suggest 160C-180C and other datasheets suggest upto 260C for reflow.

    I built the unit with Fibro-insulation, it gets to 275C

    I carefully put my loaded PCB and ran it up to 250C

    it worked, but I had to adjust some parts. I put that board through 7 times at over 200C

    it still worked at 25MHz, albeit scorched with a tinge of burnt.

    the moral of the story is that the temp is not critical for prototypes.

    Lead free you need over 200C

    Leaded solder needs over 190C to flow well.  ( 2 minutes duration)

    Capacitors don't like the high temp, the capacity will degrade with excessive temperature.

    I use through-hole caps for that reason.