cancel
Showing results for 
Search instead for 
Did you mean: 

Header Pins that are free on stm32f407vgt6 board.

Phillips Jr..Clyde
Associate III
Posted on November 08, 2012 at 19:00

My hardware guy tells me that most of the SOC peripherals don't make it out to the header pins on this board. He says they are tied up with board supported peripherals.

1) In general is this true? Is this board designed to allow external hobbyist bread boarding, where one plays with the internal periphs like counter/timers, gpio, etc?

2) Where are the ''actually available'' connections documented.

3) Here is the list of what we need...

I have done a serial uart loopback test already so I though that part was good but he says one the boards push-button is connected and just not interferring....

1. 32 bit timer frequency input

2. One capture pin for the 32 bit timer chosen. 

3. A divider (by 32000) that can use the input from the 32 bit timer

4. An output pin for that divider

5. A UART I/O 2 pins

6. An I2C I/O  2 pins

7. Two GP input pins.

He told me:

I can't find it. (them)

Thanks in advance!

#header-pins
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Andrew Neil
Super User
Posted on November 08, 2012 at 20:29

All the board documentation is here:

http://www.st.com/internet/evalboard/product/252419.jsp

The User Manual contains schematics and pinout tables:

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00039084.pdf

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on November 08, 2012 at 23:40

It has a reasonable mix of internal and external peripherals.

Using a couple of USART, with SDIO and TIMs here. You'd have to do your own due diligence via the schematic and user manuals to see what you can or can't get out. People have posted Excel sheets before, and there was a MicroExplorer tool.

These boards will always be a compromise, a feature fit for one individual is a bane for others.  Generally you're not going to be able to escape all peripherals simultaneously, or do DMA to all channels/devices, and you might have to do some juggling to get the mix or subset you want. The F4 parts have a more flexible muxing scheme than the older F1 parts.

If you want more of a breakout board there have been several on eBay, including unpopulated PCB for a couple of dollars. The chips also come in high pin-count packages to help escape peripherals.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Phillips Jr..Clyde
Associate III
Posted on November 09, 2012 at 02:06

Thanks. The UM has the scary details. We will have to test out that all the muxed signals don't interact/interfere with our use.