cancel
Showing results for 
Search instead for 
Did you mean: 

Having problem with UART communication in Interrupt mode

SLuit.1
Associate III

I am doing a project on STM32H747 DISCO Discovery board involving UART. I am sending one string continuoulsy with 5 seconds delay from esp32 to stm32. I am able to receive the string in polling mode but I am not able to receive the string in Interrupt mode.

I am using UART 8 and I have configure GPIO for the pins as follows:

static void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct;

 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOJ_CLK_ENABLE();

 /*Configure GPIO pin: PJ8   For D1 pin for TX */

 GPIO_InitStruct.Pin = GPIO_PIN_8;

 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

 //GPIO_InitStruct.Pull = GPIO_NOPULL; //pullup

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

 GPIO_InitStruct.Alternate = GPIO_AF8_UART8;

 HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct);

 /*Configure GPIO pin: PJ9   For D0 pin for RX */

 GPIO_InitStruct.Pin = GPIO_PIN_9;

 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; //MODE_ALTERNATE?

 //GPIO_InitStruct.Pull = GPIO_NOPULL; //or NOPULL?

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

 GPIO_InitStruct.Alternate = GPIO_AF8_UART8;

 HAL_GPIO_Init(GPIOJ, &GPIO_InitStruct);

}

I have initialised the UART as follow:

void MX_UART8_Init(void){

//Peripheral clock enable

__HAL_RCC_UART8_CLK_ENABLE();

__HAL_UART_CLEAR_IDLEFLAG(&huart8);

__HAL_UART_ENABLE_IT(&huart8, UART_IT_IDLE); //Enable serial port idle interrupt

huart8.Instance = UART8;

huart8.Init.BaudRate = 115200;

huart8.Init.WordLength = UART_WORDLENGTH_8B;

huart8.Init.StopBits = UART_STOPBITS_1;

huart8.Init.Parity = UART_PARITY_NONE;

huart8.Init.Mode = UART_MODE_TX_RX;

huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart8.Init.OverSampling = UART_OVERSAMPLING_16;

huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;

huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;

huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

HAL_UART_Init(&huart8);

if (HAL_UART_Init(&huart8) != HAL_OK)

 {

  Error_Handler();

 }

//UART8 Idle Interrupt Configuration

HAL_NVIC_SetPriority(UART8_IRQn, 1, 1);

HAL_NVIC_EnableIRQ(UART8_IRQn);

}

I called the function below before while(1) loop inside main:

 HAL_UART_Receive_IT (&huart8, (uint8_t*) &Rx_data, sizeof(Rx_data));

I called this complete interrupt function and tried to print some string to terminal once it is triggered.

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)

{

if(huart->Instance == UART8 ){

  HAL_UART_Receive_IT(&huart8, (uint8_t*) &Rx_data, sizeof(Rx_data));

  HAL_UART_Transmit(&huart3,(void*)"Data Received\r\n",15, 100);

}

}

Do I need to enable or configure something somewhere else in the library as well to make the interrupt work. I could not found any document regarding it . The only thing that I have found while surfing on the internet and example projects are the things that I have explained above.

Could you please help me out with it and let me know the problem as I am having problem with such a simple thing.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @SLuit.1​ ,

Have a look at this FAQ STM32 UART DMA RX/TX, it may be helpful for you.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
waclawek.jan
Super User

> I am not able to receive the string in Interrupt mode.

What are the symptoms? Is the ISR called at all?

> HAL_UART_Transmit(&huart3,(void*)"Data Received\r\n",15, 100);

It's not a good idea to call a lengthy blocking function in the ISR.

JW