cancel
Showing results for 
Search instead for 
Did you mean: 

Hardfault while using TrustZone STM32H573i-DK

funkii
Associate III

Hi everyone,

I'm currently experimenting with a STM32H573i-DK and TrustZone and facing some issues.

First I tried enabling TrustZone in the Project Creation Process. When i try to run this empty project using the steps:

Spoiler
  • Select and build the xxxxx_NS project, this will automatically trigger build of xxxxx_S project
  • Select the xxxxx_S project and select “Debug configuration”
    • Double click on “STM32 Cortex-M C/C++ Application”
    • Select “Startup” > “Add” >
  • Select the xxxxx_NS project
  • Build configuration : Select Release/Debug
  • Click Debug to debug the example

 

the execution lands in the HardFault_Handler after the call to NonSecure_Init().

 

Almost the same happens if I try to run the GTZC_MPCWM_IllegalAccess_TrustZone example. 

After the call to SECURE_SAU_MPCWM_SetInitConfig(), the execution lands in the HardFault_Handler().

I'm following the steps at the bottom of the Readme file.

 

Am I missing something or has anyone got an explanation for this behaviour?

I would appreciate any help or resources on this topic.

Best

funkii 

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
funkii
Associate III

I just forgot to set the Option Bytes as described in here ...

 

Spoiler


User Option Bytes configuration:

Please note the internal Flash is fully secure by default in TZEN=0xB4 and User Option Bytes SECWM1_PSTRT/SECWM1_PEND and SECWM2_PSTRT/SECWM2_PEND should be set according to the application configuration. Here the proper User Option Bytes setup in line with the project linker/scatter file is as follows: - TZEN=0xB4 - SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure - SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 meaning no page of Bank2 set as secure, hence Bank2 non-secure



View solution in original post

1 REPLY 1
funkii
Associate III

I just forgot to set the Option Bytes as described in here ...

 

Spoiler


User Option Bytes configuration:

Please note the internal Flash is fully secure by default in TZEN=0xB4 and User Option Bytes SECWM1_PSTRT/SECWM1_PEND and SECWM2_PSTRT/SECWM2_PEND should be set according to the application configuration. Here the proper User Option Bytes setup in line with the project linker/scatter file is as follows: - TZEN=0xB4 - SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure - SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 meaning no page of Bank2 set as secure, hence Bank2 non-secure