cancel
Showing results for 
Search instead for 
Did you mean: 

Handcrafted FIR routine

gdp123a
Associate II
Posted on January 16, 2009 at 03:15

Handcrafted FIR routine

#stm32l
2 REPLIES 2
gdp123a
Associate II
Posted on May 17, 2011 at 12:59

Here is my attempt at an efficient FIR routine.

It uses a long table of instructions to avoid the overhead of looping. After all, compared to the early days of micros there is plenty of space in these chips. I wasn't too impressed with the flexibility of the FIR routine

in the recent DSP library.

This filter works well with circular buffers (of any size).

Filters (of any length) can be swapped easily.

Please check the software thoroughly for errors before using - and use

at your own risk (after thorough testing).

I feel the DSP capabilties of the STM32 is one of its strengths and it is an area where ST should put more effort into.

Analog Devices are a good example to follow when it comes to DSP application notes, theory etc. (eg. Digital Signal Processing in VLSI, Digital Signal Processing Applications using the ADSP-2100 family)

Greg.

Nickname12657_O
Associate III
Posted on May 17, 2011 at 12:59

Dear Greg,

Many thanks for your excellent contribution ...

0690X0000060MkyQAE.gif and for the gift. Our local Support will be happy to assist and provide your required materials with our new STM32L devices

Cheers,

STOne-