cancel
Showing results for 
Search instead for 
Did you mean: 

__HAL_LOCK routines with no __HAL_UNLOCK

AndyJT
Associate III
Posted on November 03, 2016 at 15:39

Hi,

__HAL_LOCK has never bothered us previously with v 1.3 HAL library.

However, I have updated to 1.5.1 STM32F7 lib and found that stm32f7xx_hal_sai caused us problems.

It was related to the handle being kept locked after calling HAL_SAI_DMAStop when no DMA transfer was already happening. (ie, hdma->Lock = HAL_LOCKED)

I notice there are lots of routines which lock the SAI handle, yet return without unlocking. Shouldn't all return paths unlock the handle ??

For example:

HAL_StatusTypeDef HAL_SAI_DMAStop(SAI_HandleTypeDef *hsai)

{

  /* Process Locked */

  __HAL_LOCK(hsai);

  /* Disable the SAI DMA request */

  hsai->Instance->CR1 &= ~SAI_xCR1_DMAEN;

  /* Abort the SAI DMA Streams */

  if(hsai->hdmatx != NULL)

  {

    if(HAL_DMA_Abort(hsai->hdmatx) != HAL_OK)

    {

 // SHOULD INSERT THIS HERE ????? __HAL_UNLOCK(hsai);

      return HAL_ERROR;

    }

  }

  if(hsai->hdmarx != NULL)

  {

    if(HAL_DMA_Abort(hsai->hdmarx) != HAL_OK)

    {

 // SHOULD INSERT THIS HERE ????? __HAL_UNLOCK(hsai);

      return HAL_ERROR;

    }

  }

  

  /* Disable SAI peripheral */

  SAI_Disable(hsai);

  hsai->State = HAL_SAI_STATE_READY;

  /* Process Unlocked */

  __HAL_UNLOCK(hsai);

  return HAL_OK;

}

#stm32f7 #dogfooding
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 03, 2016 at 17:00

Shouldn't all return paths unlock the handle ??

You'd think, but the library is disappointingly poor in its implementation and testing.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..