Skip to main content
MMARI.1
Senior II
January 19, 2024
Solved

HAL_DMA_Start_IT - CALL back

  • January 19, 2024
  • 4 replies
  • 6575 views

hi,

DMA setting is in NORMAL mode 

i am getting output GPIO-C Port  via tim2_up .

HAL_DMA_Start_IT(&hdma_tim2_up, (uint32_t)pixelclock, (uint32_t)&(GPIOC->ODR), 2);

it's working fine but i need to enable call back once data is  transferred  .

the following  Xfercpltcallback is ""not working "".

 

void XferCpltCallback(DMA_HandleTypeDef *hdma)

{

flag++;

}

which  call back i need to use  for DMA data transfer completion 

 

 

 

 

 

 

This topic has been closed for replies.
Best answer by Pierre_Paris

Hello @MMARI.1 ,

Can you please share your DMA configuration ?

Here is an extract from the STM32CubeF1 FW under the root STM32Cube_FW_F1_V1.8.0\Projects\STM3210E_EVAL\Examples\DMA\DMA_FLASHToRAM :

static void DMA_Config(void)
{
 /*## -1- Enable DMA1 clock #################################################*/
 __HAL_RCC_DMA1_CLK_ENABLE();

 /*##-2- Select the DMA functional Parameters ###############################*/
 DmaHandle.Init.Direction = DMA_MEMORY_TO_MEMORY; /* M2M transfer mode */
 DmaHandle.Init.PeriphInc = DMA_PINC_ENABLE; /* Peripheral increment mode Enable */
 DmaHandle.Init.MemInc = DMA_MINC_ENABLE; /* Memory increment mode Enable */
 DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; /* Peripheral data alignment : Word */
 DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; /* memory data alignment : Word */
 DmaHandle.Init.Mode = DMA_NORMAL; /* Normal DMA mode */
 DmaHandle.Init.Priority = DMA_PRIORITY_HIGH; /* priority level : high */

 /*##-3- Select the DMA instance to be used for the transfer : DMA1_Channel1 #*/
 DmaHandle.Instance = DMA_INSTANCE;

 /*##-4- Initialize the DMA stream ##########################################*/
 if(HAL_DMA_Init(&DmaHandle) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler(); 
 }

 /*##-5- Select Callbacks functions called after Transfer complete and Transfer error */
 HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_CPLT_CB_ID, TransferComplete);
 HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_ERROR_CB_ID, TransferError);

 /*##-6- Configure NVIC for DMA transfer complete/error interrupts ##########*/
 /* Set Interrupt Group Priority */
 HAL_NVIC_SetPriority(DMA_INSTANCE_IRQ, 0, 0);

 /* Enable the DMA STREAM global Interrupt */
 HAL_NVIC_EnableIRQ(DMA_INSTANCE_IRQ);

 /*##-7- Start the DMA transfer using the interrupt mode ####################*/
 /* Configure the source, destination and buffer size DMA fields and Start DMA Channel transfer */
 /* Enable All the DMA interrupts */
 if (HAL_DMA_Start_IT(&DmaHandle, (uint32_t)&aSRC_Const_Buffer, (uint32_t)&aDST_Buffer, BUFFER_SIZE) != HAL_OK)
 {
 /* Transfer Error */
 Error_Handler();
 }
}

 Have you respected the 7 steps ?

Best Regards,

Pierre

4 replies

Pierre_Paris
Pierre_ParisBest answer
ST Employee
January 19, 2024

Hello @MMARI.1 ,

Can you please share your DMA configuration ?

Here is an extract from the STM32CubeF1 FW under the root STM32Cube_FW_F1_V1.8.0\Projects\STM3210E_EVAL\Examples\DMA\DMA_FLASHToRAM :

static void DMA_Config(void)
{
 /*## -1- Enable DMA1 clock #################################################*/
 __HAL_RCC_DMA1_CLK_ENABLE();

 /*##-2- Select the DMA functional Parameters ###############################*/
 DmaHandle.Init.Direction = DMA_MEMORY_TO_MEMORY; /* M2M transfer mode */
 DmaHandle.Init.PeriphInc = DMA_PINC_ENABLE; /* Peripheral increment mode Enable */
 DmaHandle.Init.MemInc = DMA_MINC_ENABLE; /* Memory increment mode Enable */
 DmaHandle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; /* Peripheral data alignment : Word */
 DmaHandle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; /* memory data alignment : Word */
 DmaHandle.Init.Mode = DMA_NORMAL; /* Normal DMA mode */
 DmaHandle.Init.Priority = DMA_PRIORITY_HIGH; /* priority level : high */

 /*##-3- Select the DMA instance to be used for the transfer : DMA1_Channel1 #*/
 DmaHandle.Instance = DMA_INSTANCE;

 /*##-4- Initialize the DMA stream ##########################################*/
 if(HAL_DMA_Init(&DmaHandle) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler(); 
 }

 /*##-5- Select Callbacks functions called after Transfer complete and Transfer error */
 HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_CPLT_CB_ID, TransferComplete);
 HAL_DMA_RegisterCallback(&DmaHandle, HAL_DMA_XFER_ERROR_CB_ID, TransferError);

 /*##-6- Configure NVIC for DMA transfer complete/error interrupts ##########*/
 /* Set Interrupt Group Priority */
 HAL_NVIC_SetPriority(DMA_INSTANCE_IRQ, 0, 0);

 /* Enable the DMA STREAM global Interrupt */
 HAL_NVIC_EnableIRQ(DMA_INSTANCE_IRQ);

 /*##-7- Start the DMA transfer using the interrupt mode ####################*/
 /* Configure the source, destination and buffer size DMA fields and Start DMA Channel transfer */
 /* Enable All the DMA interrupts */
 if (HAL_DMA_Start_IT(&DmaHandle, (uint32_t)&aSRC_Const_Buffer, (uint32_t)&aDST_Buffer, BUFFER_SIZE) != HAL_OK)
 {
 /* Transfer Error */
 Error_Handler();
 }
}

 Have you respected the 7 steps ?

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MMARI.1
MMARI.1Author
Senior II
January 20, 2024

 

DMA configuration Memory to Perpheral

 

static void MX_DMA_Init(void)

{

 

/* DMA controller clock enable */

__HAL_RCC_DMA1_CLK_ENABLE();

 

/* DMA interrupt init */

/* DMA1_Channel2_IRQn interrupt configuration */

HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);

 

}

 

void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)

{

if(htim_base->Instance==TIM2)

{

/* USER CODE BEGIN TIM2_MspInit 0 */

 

/* USER CODE END TIM2_MspInit 0 */

/* Peripheral clock enable */

__HAL_RCC_TIM2_CLK_ENABLE();

 

/* TIM2 DMA Init */

/* TIM2_UP Init */

hdma_tim2_up.Instance = DMA1_Channel2;

hdma_tim2_up.Init.Direction = DMA_MEMORY_TO_PERIPH;

hdma_tim2_up.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_tim2_up.Init.MemInc = DMA_MINC_ENABLE;

hdma_tim2_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

hdma_tim2_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

hdma_tim2_up.Init.Mode = DMA_NORMAL;

hdma_tim2_up.Init.Priority = DMA_PRIORITY_LOW;

if (HAL_DMA_Init(&hdma_tim2_up) != HAL_OK)

{

Error_Handler();

}

 

__HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim2_up);

 

/* USER CODE BEGIN TIM2_MspInit 1 */

 

/* USER CODE END TIM2_MspInit 1 */

}

 

}

 

 

 

TDK
January 19, 2024

hdma->XferCpltCallback gets called from HAL_DMA_IRQHandler which should be called from within the actual DMA IRQ handler. Are you doing that? It should be in your stm32fxxx_it.c file.

"If you feel a post has answered your question, please click ""Accept as Solution""."
MMARI.1
MMARI.1Author
Senior II
January 20, 2024

 Now callback is happening via stm32fxxx_it.c ->HAL_DMA_IRQHandler

 

 

void DMA1_Channel2_IRQHandler(void)

{

/* USER CODE BEGIN DMA1_Channel2_IRQn 0 */

 

/* USER CODE END DMA1_Channel2_IRQn 0 */

HAL_DMA_IRQHandler(&hdma_tim2_up);

/* USER CODE BEGIN DMA1_Channel2_IRQn 1 */

flag++;

 

/* USER CODE END DMA1_Channel2_IRQn 1 */

}