cancel
Showing results for 
Search instead for 
Did you mean: 

GPS receiver for P-NUCLEO-LRWAN1

Apostolos Staridis
Associate
Posted on May 17, 2017 at 18:38

Hello,

I am working with the board P-NUCLEO-LRWAN1 (

https://community.st.com/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fevaluation-tools%2Fp-nucleo-lrwan1.html

) for a project. I want to add a GPS receiver to that board for the purpose of that project . Can you tell me which one I should choose ? And how difficult is to get NMEA data ?

Thank you in advance

4 REPLIES 4
Posted on May 17, 2017 at 18:55

I'm using the DISCO board, but a shield like this should suffice. On the Nucleo-64 D0/D1 has some conflict with the ST-LINK VCP but you might have other pin choices

Removing link for Duinopeak GPS Shield NEO-6M to break the moderation on this post..

NMEA data starts automatically at 9600 8N1, connect it to a few USART input.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 17, 2017 at 21:42

http://www.ebay.com/itm/Duinopeak-NEO-6M-GPS-Shield-for-Arduino-with-GPS-Antenna-/272137634759

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 18, 2017 at 08:50

NMEA data starts automatically at 9600 8N1, connect it to a few USART input.

I know boards that use a different default baudrate. Just check the manual.

Usually, the baudrate can be switched at runtime, and NMEA sentences can be turned on/off.

Posted on May 18, 2017 at 17:27

Some older GPS were 4800 baud (think 1980's era designs/compatibility), but the data stream typically generated in the last decade overwhelms that.

Both the NEO-6M and NEO-M8N, and similar variants, all support 9600 baud by default, but can be reconfigured

YMMV, but always RTFM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..