2019-04-30 6:51 AM
Dear Member
I tried to get date from GPRMC, but not getting any response:
code :
sscanf(str,"$GPRMC,%s,%2hhd%2hhd%2hhd,%c,%f,%c,%f,%c,%f,%c,%f,%f,%2hhd%2hhd%2hhd,%f,%c,%c,*%2s\r\n",&GPS.GPRMC.xxRMC,&GPS.GPRMC.UTC_Hour,&GPS.GPRMC.UTC_Min,&GPS.GPRMC.UTC_Sec,&GPS.GPRMC.status,&GPS.GPRMC.Latitude,&GPS.GPRMC.NS_Indicator,&GPS.GPRMC.Longitude,&GPS.GPRMC.EW_Indicator,&GPS.GPRMC.spd,&GPS.GPRMC.cog,&GPS.GPRMC.UTC_Day,&GPS.GPRMC.UTC_Month,&GPS.GPRMC.UTC_Year,&GPS.GPRMC.mv,&GPS.GPRMC.mvEW,&GPS.GPRMC.posMode,&GPS.GPRMC.CheckSum);Am I missing something here ?
Thanks
2019-05-02 9:33 PM
$GPGGA,043139.00,3208.00593,S,11559.31050,E,1,11,0.80,33.1,M,-30.6,M,,*54
$GPGSA,A,3,11,23,31,08,32,18,22,01,03,14,17,,1.27,0.80,0.98*0D
$GPGSV,4,1,15,01,83,198,34,03,54,216,31,08,14,351,29,09,09,312,*71
$GPGSV,4,2,15,11,66,329,35,14,24,137,29,17,19,230,29,18,67,042,26*76
$GPGSV,4,3,15,19,04,214,14,22,63,174,16,23,43,309,33,31,33,102,32*78
$GPGSV,4,4,15,32,09,136,28,42,41,046,,50,41,046,*48
$GPGLL,3208.00593,S,11559.31050,E,043139.00,A,A*70
$GPRMC,043140.00,A,3208.00595,S,11559.31048,E,0.046,,030519,,,A*64
$GPVTG,,T,,M,0.046,N,0.086,K,A*2F
$GPGGA,043140.00,3208.00595,S,11559.31048,E,1,11,0.80,33.1,M,-30.6,M,,*55
$GPGSA,A,3,11,23,31,08,32,18,22,
looks like strstr can not parse the line after \r\n ....GPVTG is on the bottom...do you reckon ? thanks
2019-05-02 10:28 PM
I never used clib str functions for parsing such long strings.
Instead, I did the following:
- check for proper sentence type ($GPRMC) string, and proper termination (\r\n).
- count comma characters, until you reach the parameter(s) you need.
- extract (up to the next comma) and convert (e.g. sscanf()).
You also need to evaluate the fix state field, i.e. if a proper position fix occured.
2019-05-03 12:00 AM
the complete code, it works on GPGGA, but doesn't work with GPVTG ....I have no clue ??? anyone ?
if( (HAL_GetTick()-GPS.LastTime>50) && (GPS.rxIndex>0))
{
char *str,*str2;
#if (_GPS_DEBUG==1)
printf("%s",GPS.rxBuffer);
#endif
str=strstr((char*)GPS.rxBuffer,"$GPVTG,");
printf(str);printf("\r\n");
if(str!=NULL)
{
memset(&GPS.GPVTG,0,sizeof(GPS.GPVTG));
sscanf(str,"$GPVTG,%f,%c,%f,%c,%f,%c,%f,%c,*%2s\r\n",
&GPS.GPVTG.cogt,&GPS.GPVTG.T,&GPS.GPVTG.cogm,&GPS.GPVTG.M,
&GPS.GPVTG.knots,&GPS.GPVTG.N,&GPS.GPVTG.kph,&GPS.GPVTG.K,
&GPS.GPVTG.CheckSum);
//$GPVTG,,T,,M,0.069,N,0.128,K,A*27 = 9 field ,spd = field7
//printf(str);printf("\r\n");
printf("======================GPVTG PARSING =================\r\n");
printf("Speed knots : %f N \r\n",GPS.GPVTG.knots);
printf("Speed in km/h : %f km/h \r\n",GPS.GPVTG.kph);
printf("====================== D O N E !=================\r\n");
HAL_Delay(500);
HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5);
}
str=strstr((char*)GPS.rxBuffer,"$GPGGA,");
//str2=str;
if(str!=NULL)
{
memset(&GPS.GPGGA,0,sizeof(GPS.GPGGA));
sscanf(str,"$GPGGA,%2hhd%2hhd%2hhd.%3hd,%f,%c,%f,%c,%hhd,%hhd,%f,%f,%c,%hd,%s,*%2s\r\n",&GPS.GPGGA.UTC_Hour,&GPS.GPGGA.UTC_Min,&GPS.GPGGA.UTC_Sec,&GPS.GPGGA.UTC_MicroSec,&GPS.GPGGA.Latitude,&GPS.GPGGA.NS_Indicator,&GPS.GPGGA.Longitude,&GPS.GPGGA.EW_Indicator,&GPS.GPGGA.PositionFixIndicator,&GPS.GPGGA.SatellitesUsed,&GPS.GPGGA.HDOP,&GPS.GPGGA.MSL_Altitude,&GPS.GPGGA.MSL_Units,&GPS.GPGGA.AgeofDiffCorr,GPS.GPGGA.DiffRefStationID,GPS.GPGGA.CheckSum);
//printf(str);printf("\r\n");
if(GPS.GPGGA.NS_Indicator==0)
GPS.GPGGA.NS_Indicator='-';
if(GPS.GPGGA.EW_Indicator==0)
GPS.GPGGA.EW_Indicator='-';
if(GPS.GPGGA.Geoid_Units==0)
GPS.GPGGA.Geoid_Units='-';
if(GPS.GPGGA.MSL_Units==0)
GPS.GPGGA.MSL_Units='-';
GPS.GPGGA.LatitudeDecimal=convertDegMinToDecDeg(GPS.GPGGA.Latitude);
GPS.GPGGA.LongitudeDecimal=convertDegMinToDecDeg(GPS.GPGGA.Longitude);
perth_hour = GPS.GPGGA.UTC_Hour + 8;
printf("======================B E G I N =================\r\n");
printf("NEO 6M GPS MODULE INIT....\r\n");
printf("UTC TIME %u ",GPS.GPGGA.UTC_Hour);
printf(": %u :",GPS.GPGGA.UTC_Min);
printf(" %u \r\n",GPS.GPGGA.UTC_Sec);
printf("Perth TIME %u ",perth_hour);
printf(": %u :",GPS.GPGGA.UTC_Min);
printf(" %u \r\n",GPS.GPGGA.UTC_Sec);
printf("Altitude: %lf m\r\n",GPS.GPGGA.MSL_Altitude);
printf("Latitude is %lf \r\n",GPS.GPGGA.LatitudeDecimal);
printf("North South Indicator, (S)South (N)North is %c",GPS.GPGGA.NS_Indicator);
printf("\r\n");
printf("Longitude is %lf ",GPS.GPGGA.LongitudeDecimal);
printf("\r\n");
printf("West East Indicator, (W)West (E)East is %c \r\n",GPS.GPGGA.EW_Indicator);
printf("Satellites Used : %d \r\n",GPS.GPGGA.SatellitesUsed);
printf("===================================================\r\n");
//test_card();
}
2019-05-03 12:02 AM
I got from printf on line 10
$GPVTG,,T,,M,0.074,N,0.138,K,A*2A
$GPGGA,070050.00,3208.00548,S,11559.30824,E,1,10,0.82,36.0,M,-30.6,M,,*51
$GPGSA,A,3,23,26,06,09,22,01,03,16,19,07,,,1.52,0.82,1.28*05
$GPGSV,5,1,17,01,21,009,23,02,01,214,,03,52,084,37,04,40,264,31*7B
$GPGSV,5,2,17,06,33,233,35,07,40,341,25,09,54,244,28,11,04,005,*79
$GPGSV,5,3,17,16,15,089,12,17,06,297,,19,09,273,27,22,32,066,32*76
$GPGSV,5,4,17,23,60,164,35,26,12,117,21,30,09,332,19,42,41,046,*7E
$GPGSV,5,5,17,50,41,046,*4D
$GPGLL,3208.00548,S,11559.30824,E,070050.00,A,A*72
$GPRMC,070051.00,A,3208.00541,S,11559.30818,E,0.146,,030519,,,A*61
$GPVTG,,T,,M,0.146,N,0.271,K,A*24
$GPGGA,070051.00,3208.00541,S,11559.30818,E,1,10,0.82,36.1,M,-30.6,M,,
2019-05-03 12:45 AM
This what I got from function ProcessNMEALine((char*)GPS.rxBuffer)
DecodeNMEA
$GPRMC,074341.00,A,3208.00668,S,11559.30844,E,0.029,,030519,,,A*6E
$GPVTG,,T,,M,0.029,N,0.055,K,A*28
$GPGGA,074341.00,3208.00668,S,11559.30844,E,1,10,0.79,32.5,M,-30.6,M,,*54
$GPGSA,A,3,23,02,26,06,09,22,03,16,07,30,,,1.46,0.79,1.23*07
$GPGSV,4,1,15,01,03,012,,02,14,225,25,03,38,061,31,04,50,239,31*7A
$GPGSV,4,2,15,06,41,255,36,07,62,333,32,09,60,209,42,16,20,108,28*7A
$GPGSV,4,3,15,19,00,290,,22,17,053,20,23,49,137,35,26,09,134,20*7D
$GPGSV,4,4,15,30,27,326,37,42,41,046,,50,41,046,*4B
$GPGLL,3208.00668,S,11559.30844,E,074341.00,A,A*72
$GPRMC,074342.00,A,3208.00667,S,11559.30843,E,0.057,,030519,,,A*6C
$GPVTG,,T,,M,0.057,N,0.106,K,A*26
$GPGGA,074342.00,3208.00667,S,11559.30843,E,1,10,0.79,32.6,M,-30.6,M,,*5C
$GPGSA,A,3,23,02,26,06,09,22,03,16,07
Fields 13
#00 : $GPRMC
#01 : 074341.00
#02 : A
#03 : 3208.00668
#04 : S
#05 : 11559.30844
#06 : E
#07 : 0.029
#08 :
#09 : 030519
#10 :
#11 :
#12 : A
2019-05-03 1:03 AM
Hi,
scanf works for fixed length and format messages.
Depending on sentence validity or fix validity or state (A or V , 2D,3D,etc) the sentences may change length by omitting fields and change signs.
Also for different versions of NMEA output the decimal part of Latitude and Longitude can vary from 2 to 5 digits.
An option is to feed raw data to a State Machine and by byte per byte process to extract Talker, Command, Data fields, Checksum or other proprietary data. Using an atoi function can convert arithmetical fields to numbers.