cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO usage when ADC is enabled

davidhauser
Associate II
Posted on May 21, 2008 at 20:29

GPIO usage when ADC is enabled

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
davidhauser
Associate II
Posted on May 17, 2011 at 12:35

Hey

I'd like to use the ADC1 (Channel5 on PA.05). Is it possible to use PA.00 (which would be Channel0 of the ADC1) as an floating input? Or is it blocked by ADC1?

Thanks for your help

lanchon
Associate III
Posted on May 17, 2011 at 12:35

sure, just don't configure it as analog input.