2015-08-21 7:11 PM
Is there a document that describes the selection of push pull, open drain,
maximum output speed, AHB clock, etc for GPIO port operation on STM32F427xx under STM32CubeMX ? The datasheets for the chips on the PCB to which the GPIO pins are connected do not state explicitly a requirement of one or the other of these PIO configuration selections. I am not seeing any output, though the RCC clock is activation and another port is inputting successfully. #gpio-output-drain-push-pull2015-08-22 4:06 AM
Hi Aeneas,
I'd highly recommend you to refer to thishttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00104712.pdf
about STM32CubeMX for STM32 configuration and initialization C code generation.In the paragraph “GPIO Configuration window�, you find how to configure the settings of the GPIO pins.-Syrine-2015-08-22 2:25 PM
That document section referenced does not describe what the STM32
circuitry is doing differently under each choice and under which circumstances, connected to what sorts of devices, each choice of GPIO configuration it presents should be selected.2015-08-22 8:52 PM
Push-Pull and Open-Drain are concepts beyond the STM32, you'd pick the appropriate one for the interface/device you're attaching them too.
The ''speed'' is a bit different, it actually relates the slew-rate of the pin, ie how aggressively the pin is driven high/low. It's going to depend on what exactly you're driving the signal into, and the load it presents. A serial point is only going to need a 1 or 2 MHz setting.2015-08-23 12:58 PM
A
bout
push-pull
and
open drain
:
http://coactionos.com/embedded%20design%20tips/2013/10/21/Tips-Understanding-Microcontroller-Pin-Input-Output-Modes/2015-08-25 2:25 PM
After experimenting with the different GPIO configuration options, I did not notice
much difference in output voltage measurements. In all cases, I am seeing all of my data pins transition between 3.3V and maybe 3V, instead of 3.3V to Ground, (if they show transition at all). The span of high to low voltages is contrained by some sort of electrical issue, whether it is configuration of the STM32 chip or from outside, is still unclear.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.