Get more resolution from RTC clock
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-02 1:28 AM
Hello there,
I was wondering either it is possible to count with microseconds resolution isntead of seconds resolution using RTC 32k clock? I am using HAL lib. In theRTC_TimeTypeDef time structure there are 2 members I dont quite understand:/*!< Specifies the RTC_SSR RTC Sub Second register content.
This parameter corresponds to a time unit range between [0-1] Second
with [1 Sec / SecondFraction +1] granularity */
uint32_t SubSeconds;
/*!< Specifies the range or granularity of Sub Second register content
corresponding to Synchronous pre-scaler factor value (PREDIV_S)
This parameter corresponds to a time unit range between [0-1] Second
with [1 Sec / SecondFraction +1] granularity.
This field will be used only by HAL_RTC_GetTime function */
uint32_t SecondFraction;
At the begining I thought I would be able to use them somehow to specify the time with more precision, but those values dont change.
I would apreciate all help in this case.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-06 11:21 PM
Clive, you example is using SPL which has different struct for RTC than HAL.
Thomas, i tired your example but I dont think it works correctly. The msec part nearly always returns the same value, each time I reset the mcu and retreive some startup logs the msec value is incremented by one, something is wrong.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-07 2:37 AM
Hello,
hardware ? ,cpu ?, library version ?
I use STM32F429 , LSE with 32.768Khz crystal
void
SystemClock_Config
(
void
)
{
…
PeriphClkInitStruct
.PeriphClockSelection = RCC_PERIPHCLK_SAI_PLLI2S|RCC_PERIPHCLK_RTC;
PeriphClkInitStruct
.PLLI2S.PLLI2SN = 192;
PeriphClkInitStruct
.PLLI2S.PLLI2SQ = 2;
PeriphClkInitStruct
.PLLI2SDivQ = 2;
PeriphClkInitStruct
.
RTCClockSelection
= RCC_RTCCLKSOURCE_LSE;
HAL_RCCEx_PeriphCLKConfig(&
PeriphClkInitStruct
);
…
}
hrtc.
Init
.
AsynchPrediv
= 31;
hrtc.
Init
.
SynchPrediv
= 1023;
with LSI = 32.000Khz crystal, you should usehrtc.
Init
.
AsynchPrediv
= 31;
hrtc.
Init
.
SynchPrediv
= 999;
I use following code
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
msec = 999 - (sTime.
SubSeconds
* 999 / sTime.
SecondFraction
);
test code ...RTC_TimeTypeDef
sTime;
RTC_DateTypeDef
sDate;
tsprintf(
''RCC->BDSR=0x%04x RTCEN:0x%1x RTCSEL:0x%1x (1=LSE,2=LSI,3=HSE)\r\n''
,RCC->BDCR,((RCC->BDCR)>>15)&0x01,((RCC->BDCR)>>8)&0x03);
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
tsprintf(
''stime.SecondFraction=%d \r\n''
,sTime.
SecondFraction
);
tsprintf(
''here we start\r\n''
);
os
Delay(10);
// we use freeRtos else use HAL_Delay()
tsprintf(
''after 10
ms
delay\r\n''
);
osDelay(20);
tsprintf(
''after 20
ms
delay\r\n''
);
osDelay(50);
tsprintf(
''after 50
ms
delay\r\n''
);
os
Delay(100);
tsprintf(
''after 100
ms
delay\r\n''
);
osDelay(200);
tsprintf(
''after 200
ms
delay\r\n''
);
osDelay(500);
tsprintf(
''after 500
ms
delay\r\n''
);
osDelay(1000);
tsprintf(
''after 1000
ms
delay\r\n''
);
this prints with LSE
...
2015-12-07 11:02:58.005 RCC->BDSR=0x8103 RTCEN:0x1 RTCSEL:0x1 (1=LSE,2=LSI,3=HSE)
2015-12-07 11:02:58.005 stime.SecondFraction=1023
2015-12-07 11:02:58.005 here we start
2015-12-07 11:02:58.016 after 10 ms delay
2015-12-07 11:02:58.036 after 20 ms delay
2015-12-07 11:02:58.085 after 50 ms delay
2015-12-07 11:02:58.186 after 100 ms delay
2015-12-07 11:02:58.386 after 200 ms delay
2015-12-07 11:02:58.886 after 500 ms delay
2015-12-07 11:02:59.886 after 1000 ms delay
…
with LSI
...
2015-12-07 11:24:41.005 RCC->BDSR=0x8203 RTCEN:0x1 RTCSEL:0x2 (1=LSE,2=LSI,3=HSE)
2015-12-07 11:24:41.005 stime.SecondFraction=999
2015-12-07 11:24:41.005 here we start
2015-12-07 11:24:41.017 after 10 ms delay
2015-12-07 11:24:41.038 after 20 ms delay
2015-12-07 11:24:41.092 after 50 ms delay
2015-12-07 11:24:41.200 after 100 ms delay
2015-12-07 11:24:41.415 after 200 ms delay
2015-12-07 11:24:41.954 after 500 ms delay
2015-12-07 11:24:43.030 after 1000 ms delay
...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-07 7:59 AM
Clive, you example is using SPL which has different struct for RTC than HAL.
Indeed, because I'm not using HAL, mainly because it's a very thick, and often broken, PoS, but that's a whole other discussion. My goal here however, is to illustrate that the HW works just fine, so any issues you may be having with it are in the SW domain, either yours or your choice of abstraction. I think the math and methods I have addressed will port to the HAL paradigm.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-07 9:09 AM
Thank you guys, I understand how to do it now but it still seems to give me wrong output, I will post my code soon.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-12-08 2:20 AM
After closer look everything works. Thank you very much for help guys.

- « Previous
-
- 1
- 2
- Next »