cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC and GPIO Pins-

jschatz
Associate II
Posted on August 18, 2009 at 20:31

FSMC and GPIO Pins-

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jschatz
Associate II
Posted on May 17, 2011 at 13:20

When the FSMC is configured, it uses up to 25 GPIOs for its address bus. There does not appear to be any special configuration techniques to use these GPIOs except that I have set them to be outputs.

My problem, I would like to use a few of these unused address lines for inputs. If I set some of the address line GPIOs to ''input mode'', will the FSMC ignore them as address outputs?