cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS V10

GreenGuy
Lead
Posted on May 05, 2018 at 21:00

The current FreeRTOS in the Cube Repo is V8.x.x.  Way down level.  Is there a reason why the repo has not been updated to V10?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on May 05, 2018 at 21:19

Latest CubeMX packages have FreeRTOS V9.0.0. Try to update device packages as the FeeRTOS is distributed inside them.

/*

    FreeRTOS V9.0.0 - Copyright (C) 2016 Real Time Engineers Ltd.

    All rights reserved
Posted on May 06, 2018 at 02:16

The examples aren't auto-generated, changing Middlewares has significant collateral impact over many projects. If you can build your own V10 template and merge in the generated portions of the code you need it is likely to have far less regression issues.

FatFs R0.12c also isn't current.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dana Myers
Senior
Posted on July 07, 2018 at 01:07

I appreciate there's cost and risk associated with change. But I'd sure like to have access to the V10 stream buffer without tweaking my projects. I *do* appreciate that the firmware is offered basically for free so I get what I pay for.