cancel
Showing results for 
Search instead for 
Did you mean: 

Free file system

mikeprince7009
Associate II
Posted on January 03, 2012 at 07:35

Hello frnds,

      I was using Efsl with Stm32. But it is not supporting long file names.

Is der ne other free file systems which will support long file names too.

Thank you.

Mike
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
mikeprince7009
Associate II
Posted on January 03, 2012 at 07:42

rosarium
Associate II
Posted on January 03, 2012 at 08:43

yes u r right..EFSL doesn't support LFN.

You can use FAT_FS ELM from Chan. It supports LFN.

rosarium
Associate II
Posted on January 03, 2012 at 08:51

u can refer to the following link.

http://elm-chan.org/fsw/ff/00index_e.html

mikeprince7009
Associate II
Posted on January 03, 2012 at 09:23

Thnks a lot Pila.

It will help for sure.

Did you try this FS with uSD interfaced on SPI with STM32.?

disirio2
Senior
Posted on January 03, 2012 at 09:34

Hi,

The

http://www.chibios.org

project contains a demo for the STM32 with FatFS interfacing an SD/MMC card using the SPI bus.

Giovanni

rosarium
Associate II
Posted on January 03, 2012 at 09:38

u r welcome mike.

Yes I tried it with STM3210C connectivity line. FAT_FS with SPI interfaced SD. and it's working fine.