cancel
Showing results for 
Search instead for 
Did you mean: 

FMSC for NAND with INT2

gaubuali
Associate II
Posted on September 14, 2012 at 11:21

Hi all,

I am using STM3210E-EVAL.

In the User Manual, it says: ''The ready/busy signal can be connected to either WAIT signal or FSMC_INT2 signal of the STM32F103ZGT6 depending on the setting of JP7.''

I am trying to use FSMC_INT2 instead of FSMC_NWAIT but NOT successful. Only setting jumper JP7 to NWAIT works with example from ST.

Do I need to modify code to get INT2 working ?

Does anybody try that before ?

Many thanks.

Best regards,

DNN
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0