cancel
Showing results for 
Search instead for 
Did you mean: 

ADC value in interrupt

oe2
Associate III
Posted on September 14, 2012 at 14:42

I have set up interupts on the ADC1 (AWD) and ADC2(EOC). They both works well, but i'm having some concern about the values from the ADC1.

If I get an AWD interrupt, how can I then make sure that I'm getting the value from the ADC that triggers the interrupt?

Currently I read my ADC ADC_GetConversionValue(ADC1). However if I have many other interuppts with a higer priority it seems like the ADC have alredy sampled a new value before the IRQ-rutine is lanched and my triggering value is lost.

Is there a way to either stop the ADC from samping when AWD kicks in, or to get the old sample value... Any ideas?

If I put up priorit on the interupt, can I then be sure that I get the correct value...

Regards

Ola

#stm32-adc-awd-interupt
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0