cancel
Showing results for 
Search instead for 
Did you mean: 

Floating point emulation on DSP-L without floating point arithmetic

Roland Dorn
Associate II

Hi,

i am currently analyzing the FIR filter example project.

Our DSP processor supports only integer numbers. Floating point arithmetic will not be supported.

"The SoftFloat library from John Hausser is used to emulate floating point operations

on a fixed point processor (www.jhauser.us/arithmetic/SoftFloat.htm). This library is only used in combination with the CHESS front end."

As I checked the example FIR implementation the cycle add function will be realized with fmadds. The assembly command fmadds dealing with two floating point number.

 (cyclic_add function is provided by DSP-L /
 
 ST. void* cyclic_add(T* p, int offs, T* start, int len)).

The example code is dealing with floating numbers and the floating point calculation will be emulated.

Why convert the compiler the cyclic add function to a floating point assembly command?

(See attached file.)

5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @Roland Dorn​ 

In order your post reach the right people could you please clarify which STM32 chip you are using ?

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ozone
Lead III

At first glance, the assembly doesn't look like Thumb-II (Cortex M).

Hi Olivier,

it is about the STxP6016 integrated into (ST28) SR6P7x.

Kersten HEINS
Associate III

We have notified our dedicated staff in Stuttgart/Munich who will respond to you asap.

cc: @Marian GORTOL​ , @Carsten SBICK​ , @Robert BOCK​ 

I am still waiting for an answer.