FLASH LOADER DEMONSTRATOR
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-10-02 3:19 AM
Posted on October 02, 2012 at 12:19
Hy folks!
I have a problem with a STM32Discovery board, after a wrong programmation seems impossible to recover the board. I follow exactly this procedure:in switch off state connect the Boot0 Pin to 3vthen i switch on the boardnow i try to erase the memory using the flash loader demonstrator (via USART1 PA9 and PA10)when i try erasing the tool says that there are a reading protection...i try using IAR, via usb, clicking Project->Download->Erase memory but it says that there are no MCUCan you help me. please
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-10-02 6:52 AM
Posted on October 02, 2012 at 15:52
Perhaps then you need to look at what happen to the ''Option Bytes''
If you get these set wrong, it will enter various read protection modes, some irreversible. You could look to see if the Flash Loader Demonstrator can address these in the F0 boards (I assume this is what you're using, but you should be specific about which Discovery board we're talking about). The other would be to see if the ST-LINK utilities will resolve this.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..