2008-08-18 12:33 AM
Firmware Upgrade Via USART
2011-05-17 03:31 AM
Hi,
Im interested in knowing whether its possible to perform firmware upgrades via the USART. Has anyone tried it? Any directional help is appreciated. Thanks. -Mad D2011-05-17 03:31 AM
Hi mvi,
Check : : STM32F10xxx in-application programming using the USART . Enjoy using it. Cheers, STOne-32.2011-05-17 03:31 AM
2011-05-17 03:31 AM
What's the matter with this forum - why are my posts disappearing?? :-|
[ This message was edited by: st7 on 14-08-2008 16:32 ]2011-05-17 03:31 AM
Quote:
Check :
http://www.st.com/stonline/products/literature/an/13588.pdf
: STM32F10xxx in-application programming using the USART . Enjoy using it. Cheers,I'm not emjoying it at all - it's making me very frustrated!! :-| The PDF document says,Quote:
To specify the device (High-density or Medium-density) on which the software is to be run, uncomment the relative definition line in the platform_config.h header file:
//#define USE_STM3210B_EVAL //#define USE_STM3210E_EVALbut that's rubbish - because the relevant secion of platform_config.h is actually:Quote:
#if !defined (USE_STM3210B_EVAL) && !defined (USE_STM3210E_EVAL) //#define USE_STM3210B_EVAL #define USE_STM3210E_EVAL #endif (I would use the 'CODE' tags there, but that seems to be what breaks my post!) So any commenting or un-commenting of those lines will be completely ignored if either (or both) of the symbols is defined in the project - which, of course, they are!! :-| :-| The project builds cleanly immediately after downloading it from the ST site, but if the USE_STM3210E_EVAL definition in the project is changed, the build fails - saying it can't find stm32f10x_conf.h :-| :-| :-| Even if the project is then restored to exactly as it was from the site, it will not rebuild again - it continues to say that it can't find stm32f10x_conf.h :-| :-| :-| :-| If it managed to find it the first time, why can't it find it again?? :-| :-| :-| :-| :-| Leaving the definitions alone and changing the Target processor has a similar effect! :-| :-| :-| :-| :-| :-|2011-05-17 03:31 AM
Hi ST7,
keep cool, I will test it in my boards and let you back what is going there. However, when I posted my message by 22-04-2008 at that time the Application note is handling only one device family ( medium density) and the software is working fine :-| I will let you know soon, Cheers, STOne-32.2011-05-17 03:31 AM
Quote:
The project builds cleanly immediately after downloading it from the ST site, but if the USE_STM3210E_EVAL definition in the project is changed, the build fails - saying it can't find stm32f10x_conf.h
Found the cause of that - it's a Raisonance idiocy: After changing the Project properties, you have to manually save the project (or close & re-open RIDE) before doing a build - otherwise it uses the wrong include path!! :-| :-|2011-05-17 03:31 AM
The PDF documents (and readme file) state the requirement that the ''user'' application must start at 0x0800_2000.
I assume that the example projects supplied must do this, but there is no description of how it is done - which is not very helpful when it comes to creating my own application! Can you explain precisely what is needed to do this with RIDE7 ? Thanks.2011-05-17 03:31 AM
Hi ST7,
I'm not expert of Ride 8-) toolchain, I suggest you to post your messages on our Partner forums where many experts are able to help you there. I'm using Keil and IAR toolchains and the code is working fine for me :-| Cheers, ST1.