2008-10-28 05:26 AM
Firmware Library: C++ Support
2011-05-17 03:49 AM
Hi,
we are starting at the moment a large project, which will be based on several STM32 microcontrollers. We have decided to use your firmware library. We will use C++ as programming language. I am a little bit astonished that the firmware library is not really C++ compatible. All header files are missing the following keyword: extern ''C'' See e.g.http://www.parashift.com/c++-faq-lite/mixing-c-and-cpp.html#faq-32.4
And the header files are using keywords for types, which are already used by C++ itself (e.g. ''bool''). It would be greate, if you could make the header files C++ conform.2011-05-17 03:49 AM
Quote:
I am a little bit astonished that the firmware library is not really C++ compatible.
C++ is still not common in the type of small embedded projects where you might expect to find an STM32. However, as it is a new product, it is a bit remiss that they didn't at least make it compatible! :-( But they are not the only ones:http://www.luminarymicro.com/component/option,com_joomlaboard/Itemid,92/func,view/id,2918/catid,7/
2011-05-17 03:49 AM
look for a c++ build environment posted to this forum. (but it's based on fwlib 1.0.)
2011-05-17 03:49 AM
budde should be able to insert the appropriate C++ corrections into header files. The “bool� case is likely as simple s removing the typedef. But he should not have to do it.
I am not using ST’s firmware library but have an issue with IAR’s assembler vs. C++. The C++ “int xyz(void)� entry point is “xyz()� which I can not create in their assembler. It’s annoying but easy enough to get around. Except that one could then make a prototype for xyz(int) and call my assembler routine. Had I been able generate the xyz() entry point the C++ user would see a linker error and know (or should know) that something is wrong. Is there an excuse to create an STL multimap in an STM32 application? I can’t imagine one. Yet there is no reason to make it (more) difficult to accomplish. In my applications I never use general purpose memory management. Yet there is no reason why such routines should not exist.