cancel
Showing results for 
Search instead for 
Did you mean: 

FIFO in UART of STM32F767

Hemanth Sundaresh
Associate II
Posted on July 13, 2017 at 15:57

Hello All,

I wanted to know if the STM32F767, supports FIFO for the UART module? If yes, what is the size.

I need the FIFO details for configuring the Hardware flow control.

regards,

Hemanth

#uart #stm32f7 #fifo
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
AvaTar
Lead
Posted on July 13, 2017 at 16:18

I wanted to know if the STM32F767, supports FIFO for the UART module?

No.

ST's Cortex M controllers generally have no FIFO. You can use DMA instead. Actually, you are supposed to use DMA.

Check the Reference Manual.

View solution in original post

1 REPLY 1
AvaTar
Lead
Posted on July 13, 2017 at 16:18

I wanted to know if the STM32F767, supports FIFO for the UART module?

No.

ST's Cortex M controllers generally have no FIFO. You can use DMA instead. Actually, you are supposed to use DMA.

Check the Reference Manual.