cancel
Showing results for 
Search instead for 
Did you mean: 

FatFS version too old in CubeF4 library

Dulan D
Associate II
Posted on May 30, 2017 at 10:56

Hello,

By using the STM32Cube_FW_F4_V1.16.0, there is the FatFs which is provided by default as third party software. I see that the version of that FatFs is very old: R0.11. There are 6 new fixes that occurred since then and it improved things a lot. Also there is the exFat which is now supported.

Changelog:

http://elm-chan.org/fsw/ff/updates.txt

Website:

http://elm-chan.org/fsw/ff/00index_e.html

Would it be possible to update the latest release into CubeF4 middleware? I think that this should also be done with all other middleware, so people have directly the best products available freely.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on May 30, 2017 at 11:30

Hi

Burgin.Daniel

,

Your request is shared internally for further investigation.

I'll keep you update about the answer.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen