2019-05-30 12:17 AM
Hi
I am trying to write a code using STM32f103r8t6, i have installed IAR for Arm v8.40.1 i started to create a project but i could not find any library files. and then by downloading an example file i got the library files as i tried to complile i m getting the above error in the preprocessor part i have selected the target
2019-05-30 1:54 AM
Hi,
I don't use IAR anymore but I will try to help you.
In my memories, IAR is not provided with the libraries. You need to download them on the ST site.
On the view, you you selected a target device but you didn't indicate a symbol to use as preprocessor.
To define a symbol, you need to go to the "C/C++ Compiler" category and add the symbol (STM32F103xB in your case (for STM32F103R8)) in the "preprocessor" tab.
Or you can uncomment the line corresponding to your device in the file "stm32f10x.h".