cancel
Showing results for 
Search instead for 
Did you mean: 

Failing to write to SD card on SensorTile.

Armen Levonian
Associate
Posted on November 23, 2017 at 20:10

I am using the DataLog application to try to write to the SD card on the SensorTile. I have configured main.c:

LogInterface_TypeDef LoggingInterface = SDCARD_Datalog;

...changed from the default ...= USB_Datalog

In debugging the problem, I can see that in DATALOG_SD_Init...

The 'f_mount(&SDFatFs, (TCHAR const*)SDPath, 0)' fails (not equal to FR_OK).

After calling FATFS_LinkDriver(&SD_Driver, SDPath): which returns 0 (success)

SDPath = '0:/'

I am using the latest firmware:

V2.J29.M18 STM32 Debug+Mass storage

I have a 2GB Micro SD card in the SensorTile cradle.

Is anyone else having issues with this?

UPDATE: OK I have the problem solved. I replaced the 2GB SD card with a new 16GB SD card, the the DataLog app is now logging to the SD card. It seems older smaller cards are not supported.

Thanks,

Armen

0 REPLIES 0