cancel
Showing results for 
Search instead for 
Did you mean: 

F107 & LAN8720

aykutulusan
Associate II
Posted on May 09, 2016 at 09:30

Hello,

Why Lan8720A is usually used with F407, I want to use it with F107, are there

limitations

with F107?
2 REPLIES 2
Posted on May 09, 2016 at 15:16

More likely the available parts when it was originally designed. Make sure you can change the PHY address in the code, prototype the circuit you have in mind.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..