Question
EXTI interrupt on PA5 give faulty interupt at PA6(as GPIO configure).Using STM32f4 discovery kit
Posted on June 22, 2012 at 08:38
In main function when we set or reset PA6, it will land into interrupt, while I have explicitly defined in EXTI9_5_IRQHandler , that only interrupt should happen on PA5 not on PA6. I don't know what is going on Please Help??, I want PA6 as GPIO alone (not on interrupt) and PA5 input as an interrupt, plz see code below
//Code is here:::::: void EXTILine5_Config(void) { EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable GPIOA clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Enable SYSCFG clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Configure PA5 pin as input floating */ /* Connect EXTI Line5 to PA5 pin */ SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource5); /* Configure EXTI Line0 */ EXTI_InitStructure.EXTI_Line = EXTI_Line5; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable and set EXTI Line5 Interrupt to the lowest priority */ NVIC_InitStructure.NVIC_IRQChannel =EXTI9_5_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } void InitGPIOS(void) { /* Configure PA6 in output pushpull mode */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /// GPIO PA6 /* Configure PA5 in input pushpull mode */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_Init(GPIOA, &GPIO_InitStructure); } void Delay(__IO uint32_t nTime) { TimingDelay = nTime; while(TimingDelay != 0); } void TimingDelay_Decrement(void) { if (TimingDelay != 0x00) { TimingDelay--; } } void main(){ InitGPIOS(); EXTILine5_Config(); while(1) { GPIO_WriteBit(GPIOA, GPIO_Pin_6,Bit_SET); Delay(100); GPIO_WriteBit(GPIOA, GPIO_Pin_6,Bit_RESET); Delay(100); } } // GPIO Interrupt void EXTI9_5_IRQHandler(void) { if(EXTI_GetITStatus(EXTI_Line5) != RESET) { STM_EVAL_LEDToggle(LED4); EXTI_ClearITPendingBit(EXTI_Line5); } } Thanks in advance #exti-interrupt-error