cancel
Showing results for 
Search instead for 
Did you mean: 

external series resistors with OTG_HS internal PHY?

sk-st
Associate III
Posted on September 24, 2014 at 15:41

Hello,

i am designing a device only usb port with the OTG_HS of the STM32F429. In the device datasheet, the device pins DP and DM are connected dirctly to the usb-port.

In the discovery kit 32F429IDISCOVERY there are 22R series resistors used.

What to do here?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0