Skip to main content
matic
Associate III
August 7, 2016
Question

External interrupts question

  • August 7, 2016
  • 1 reply
  • 516 views
Posted on August 07, 2016 at 18:23

Hi.

Currently I use PA15 pin as external interrupt. The ISR routine is common for lines 10 through 15 and it is called EXTI15_10_IRQHandler. Now, I would like to have another signal connected to pin PB12, which has same IRQ Handler as PA15, and enable interrupt also for PB12. But I don't want to come into ISR when event on PB12 occurs. I just want to poll for the flag in EXTI->PR register. Interrupt (ISR) should occur only at event on PA15.

Is this possible or should I move one signal to different pin?

Thanks
    This topic has been closed for replies.

    1 reply

    adam23
    Associate II
    August 17, 2016
    Posted on August 17, 2016 at 09:47

    From what I saw, you have to put the signal into a different EXTI group. The pins 0-4 (I think) have their interrupts separated, EXTI9-5 and EXTI10-15 are shared and you can not find which pin it was without reading further data in ISR.