External clock generation at non-multiple of system clock
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-08 12:24 AM
Posted on April 08, 2013 at 09:24
Hi All,
I am trying to produce a 256 kHz frequency clock for use with audio codecs. I am trying to produce this 256kHz freq from the 120MHz system clock on the STM32F207 series. I would like to use the timers to produce this 256kHz clock, however 256kHz does not evenly divide into 120MHz. (120Mhz/256kHz = 468.75) Does anyone know of a way to produce a non-multiple of the system clock by using a combination of timers, and cascading timers. I have found one way to produce 192MHz from the I2S PLL, and then output on MCO 6.4MHz, which can then be divided down to 256KHz, but this requires two pins, 1 for the MCO pin and 1 for external clock input. I would prefer to be able to just use internal timers and get back two micro controller pins. Any help find a solution to this would be great. #fitter #external-clock #advanced-timers #clocks #magic-crystals #doughnuts
Labels:
- Labels:
-
TIM
This discussion is locked. Please start a new topic to ask your question.
22 REPLIES 22
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-09 5:59 AM
Posted on April 09, 2013 at 14:59
Ok lets see if I have got this right.
Currently I am out of SPI modules on the STM32. As I am using SPI for: 1) SPI Master to Flash 2) SPI For Audio to SLIC 3) SPI for another audio path But if I were to replace 1) with a Syncronous USART (that does not drive the Clock while Start/Stop bits are sent), this would give me 1 free SPI. So now I have two SPI's free for Audio to SLIC. I would use these SPI ports as follows 1) Setup 1 as an I2S module, which will act as I2S Half Duplex TX 2) Setup 2 as an I2S module slave which will act as Half Duplex RX OR 1) Setup 1 as an I2S module, which will only output a clock at 256KHz 2) Setup 2 as an SPI Slave, which will take the Clock from I2S module, and handle both TX and RX as full duplex I think that will do it. No need for some non-standard clock rate, and takes advantage of the I2S PLL's. I still keep all the SPI required functionality (albeit at a 10% slow down, but that's fine). I can even take advantage of I2S (which is fantastic!) Anyone spot any problems before I go about cutting and strapping?Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-09 6:17 AM
Posted on April 09, 2013 at 15:17
It would seem option #2 of using an SPI bus in slave mode works best, rather than using two I2S modules in half duplex.
With two in half duplex, I need to connect FRAME and CLK between the two I2S modules. This requires one more pin (the FRAME Slave pin). List of pins are: 1) I2S_MASTER_CLK 2) I2S_MASTER_FRAME 3) I2S_MASTER_TX 4) I2S_SLAVE_CLK (connected to I2S_MASTER_CLK) 5) I2S_SLAVE_FRAME (connected to I2S_MASTER_FRAME) 6) I2S_SLAVE_RX While the pin count using 1 I2S module & 1 SPI module in slave mode: 1) I2S_CLK 2) I2S_TX 3) I2S_FRAME (possibly generated by GPIO via DMA to allow SPI syncronisation) 4) SPI_SLAVE_CLK (connected to I2S_CLK) 5) SPI_SLAVE_MISOOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-04-10 12:17 AM
Posted on April 10, 2013 at 09:17
> [with USART in synchronous mode] I still keep all the SPI required functionality (albeit at a 10% slow down, but that's fine).
It's not -10% if you are after the highest attainable speeds - while the max. SPI clock is fPCLK/2, the highest USART clock is fPCLK/8, IIRC. So it's more like -90%. Whether this is detrimental in your application, I don't know. JW
- « Previous
- Next »