cancel
Showing results for 
Search instead for 
Did you mean: 

EWARM5.20

jilisegiar
Associate II
Posted on July 18, 2008 at 12:42

EWARM5.20

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
jilisegiar
Associate II
Posted on May 17, 2011 at 12:39

Hi All,

The new version of IAR(EWARM5.20A) is available now!

www.iar.com\ewarm

http://www.iar.com/website1/1.0.1.0/1070/1/index.php

Rgds

ibtissem
Associate II
Posted on May 17, 2011 at 12:39

Hi everybody,

Just to highlight that this version supports the Cortex-M3 SWV/SWO:

Cortex-M3 SWV (Single Wire Viewer) trace packets sent over the

Cortex-M3 SWO channel can be presented by the debugger.

The user have full control over the selection of trace packet types.

The communication rate is 6 MHz when using J-Link v7 or newer

(500 kHz for older J-Link versions)

Printf via SWO at the click of a button:

For Cortex-M3, printf output can be sent via the SWO channel

(that is part of the SWD interface), and displayed in the debugger

terminal I/O window. The advantage is real-time performance for debug

log messages because the CPU does not need to be halted.

To enable: Project Options>General Options>Library Configuration>Via SWO.

Enjoy it!!

jas
Associate II
Posted on May 17, 2011 at 12:39

Make sure you are using ''Y'' revision silicon STM32F10xxx chips with V5.20 otherwise you will have trouble.

http://www.st.com/stonline/products/literature/tn/14898.pdf

My IAR STM32-SK demo board will not work now with EARWM V5.20 because it has old ''B'' silicon on it.

Just found out today.

jj
Associate II
Posted on May 17, 2011 at 12:39

Never one to ''condemn'' the Arm_Wrestler to more time in the ''dungeon'' - however me doth protest...

1) Using IAR KS V 5.20

2) Have STM32-SK demo board

3) STM32 on my board is Rev ''B06'' - assume this is Rev ''B''

And it appears to WORK - and I'm using SWV - saving ''lost'' JTAG pins.

Would you be so good as to further detail, ''you will have trouble?''

Perhaps I have a different setting/set-up - be delighted if I could assist you/others...

jas
Associate II
Posted on May 17, 2011 at 12:39

OK, I'll just ignore TN0067 and this warning message then.

[ This message was edited by: Arm_Wrestler on 16-07-2008 16:58 ]

I'm having my micro pcb's stuffed today, so it was panic stations to see what version silicon had been procured.

[ This message was edited by: Arm_Wrestler on 16-07-2008 17:01 ]

jj
Associate II
Posted on May 17, 2011 at 12:39

Arm_Wrestler,

It was not my intent to challenge or impugn - I simply was reporting my recent usage/findings. (hoping that this would/could SAVE you distress/monkey-motion) Apologies if I have offended.

I can not read your post nor the jpg attachment - both are distorted.

I would be willing to load/run sample programs/code - and report my results - in the spirit of shedding additional light on your issue...

ettore
Associate II
Posted on May 17, 2011 at 12:39

Hi,

I just got a STM3210B-Eval board (loaner) and downloaded the evaluation version of IAR 5.20 but I don't have a JTAG program the board. I'm able to use DFUSE to ''upgrade'' the code in the board using the supplied images. I can successfully build the Eval demo project and generate a .hex file using the Output converter set up ''Intel Extended''. I load up DFU file manager, generate a .dfu file and ''upgrade'' the board using Dfuse. When I leave DFU mode is just goes back to DFU mode and the LCD screen is white. Is there anything I need to change in IAR to build a hex file that works with the DFU? Thanks in advance!

ettore

jj
Associate II
Posted on May 17, 2011 at 12:39

ettore:

I have 2 such eval boards - in addition to the version Arm_Wrestler mentions. Each of my STM3210B's was ''pre-loaded'' with code - the TFT lcd came to life with power up and the Leds displayed a ''chase'' pattern.

Did your board behave in this manner when you first received/powered it?

Are your Boot0/1 switches in the correct position?

Believe that there is a 40+ pg. ''Board User Guide'' available under the ''Documents'' section of this web-site. Study this & see if this helps...

jas
Associate II
Posted on May 17, 2011 at 12:39

Hi JJ

Sorry if I came over all grumpy.

I'm up to my armpits in new pcb's and unfinished f/w.

Did you try clicking on my jpg 3 times to zoom in to see the warning box clearly ?

The fact is if ST & IAR say in their TN0067:

''While running the tests with this new toolchain revision, STMicroelectronics and IAR found

some incompatibility with revisions B and Z of the STM32F10xxx Medium-density devices.

ST recommends to use the latest revision of the STM32F10xxx Medium-density, that is

revision Y.''

There must be a good reason for this and I would tend to believe them and heed their advice.

I intend to use the latest V5.20 and hence latest silicon and follow the recommended path.

I do value your knowledgeable and experienced input in this forum.

Now back to the dungeon ! :(