cancel
Showing results for 
Search instead for 
Did you mean: 

Error: junk at end of line, first unrecognized character valued 0xffffffe2

SHald.1
Associate II

I wrote the below assembly macro in startup.S file.

.macro DEBUG_ToggleLED88

  /*Enable clock to the Peripheral

   Set the pin to output

   Toggle PD14

   */

  .equ RCC_BASE, 0x58024400

  .equ GPIOD_BASE,0x58020C00

  .equ AHB4ENR_OFFSET,0x0E0‬

  .equ RCC_AHB4ENR, 0x580244E0

  .equ LED_D88_GPIO_Port,GPIOD_BASE

  .equ GPIODMODER_OFFSET,0x00

  .equ GPIODODR_OFFSET,0x14

  .equ GPIODBSRR_OFFSET, 0x18

  .equ RCC_AHB4ENR_GPIODEN_Msk,0x00000008

  .equ GPIO_MODER_MODE14_0,0x10000000

  .equ GPIO_BSRR_BS14_Msk,0x00004000

  .equ GPIO_BSRR_BR14_Msk,0x40000000

  .equ GPIOD_MODER,0x58020C00

  .equ GPIOD_ODR,0x58020C14

  .equ GPIOD_BSRR,0x58020C18

  /*RCC->AHB4ENR |= RCC_AHB4ENR_GPIODEN_Msk*/

  /*---------------------------------------*/

  /*Load address of RCC_AHB4ENR to R0*   */

  LDR        R0,=RCC_AHB4ENR

  /*LOAD the Value at address found in R0 into R1*/

  LDR        R1,[R0]

  /*Bitwise OR on the value in R1*/

  ORR        R1,#RCC_AHB4ENR_GPIODEN_Msk

  /*Store the content in R1 back at address found in R0*/

  STR        R1,[R0]

  /*GPIOD->MODER |=GPIO_MODER_MODE14_0*/

  /*--------------------------------------*/

  /*Load address of GPIOD_MODER to R0*/

  LDR        R0,=GPIOD_MODER

  /*LOAD the Value at address found in R0 into R1*/

  LDR        R1,[R0]

  /*Bitwise OR on the value in R1*/

  ORR        R1,#GPIO_MODER_MODE14_0

  /*Store the content in R1 back at address found in R0*/

  /*GPIOD->BSRR |=GPIO_BSRR_BS14_Msk*/

  /*-----------------------------------------*/

  /*Load address of GPIOD_ODR to R0*/

  LDR        R0,=GPIOD_BSRR

  /*LOAD the Value at address found in R0 into R1*/

  LDR        R1,[R0]

  /*Bitwise OR on the value in R1*/

  ORR        R1,#GPIO_BSRR_BS14_Msk

  /*Store the content in R1 back at address found in R0*/

  STR        R1,[R0]

  /*GPIOD->BSRR |=GPIO_BSRR_BR14_Msk*/

  LDR        R0,=GPIOD_BSRR

  /*LOAD the Value at address found in R0 into R1*/

  LDR        R1,[R0]

  /*Bitwise OR on the value in R1*/

  ORR        R1,#GPIO_BSRR_BR14_Msk

  /*Store the content in R1 back at address found in R0*/

  STR        R1,[R0]

.endm

But, the assembler throws the Error: junk at end of line, first unrecognized character valued 0xffffffe2

How to resolve it?

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Peter BENSCH
ST Employee

I can't explain the cause of these three ominous bytes that seem to keep slipping up. Please mark the entire macro, then delete it and reinsert it from the cleaned-up code below:

.macro DEBUG_ToggleLED88
 
   .equ RCC_BASE,0x58024400
   .equ LED_D88_GPIO_Port,0x58020C00
   .equ GPIOD_BASE,0x58020C00
   .equ GPIODODR_OFFSET,0x14
   .equ GPIODBSRR_OFFSET,0x18
   .equ RCC_AHBENR_GPIODEN_Msk,0x00000008
   .equ GPIO_MODER_MODE14_0,0x10000000
   .equ GPIO_BSRR_BS14_Msk,0x00004000
   .equ GPIO_BSRR_BR14_Msk,0x40000000
   .equ GPIOD_MODER,0x58020C00
   .equ GPIOD_ODR,0x58020C14
   .equ GPIOD_BSRR,0x58020C18
 
   LDR R0,=RCC_AHBENR
   LDR R1,[R0]
   ORR R1,#RCC_AHBENR_GPIODEN_Msk
   STR R1,[R0]
 
   LDR R0,=GPIOD_MODER
   LDR R1,[R0]
   ORR R1,#GPIO_MODER_MODE14_0
 
   LDR R0,=GPIOD_BSRR
   LDR R1,[R0]
   ORR R1,#GPIO_BSRR_BS14_Msk
   STR R1,[R0]
 
   LDR R0,=GPIOD_BSRR
   LDR R1,[R0]
   ORR R1,#GPIO_BSRR_BR14_Msk
   STR R1,[R0]
.endm

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Peter,

Thank You very much.

With the code snippet provided by you the issue got resolved.

Thank you again.

Best Regards,

Snehashis

Great!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.