cancel
Showing results for 
Search instead for 
Did you mean: 

error in adding cpp library to c project in keil

mhdizgah
Associate II
Posted on December 27, 2014 at 15:05

hi every one

im trying to develop a c project in keil ,know i need to add a cpp library file to project & it shows error,i think it is because project uses c compiler & it cant compile cpp libraries,but i dosent have any suggestion to what i must do !

keils error :

 error:  #20: identifier ''class'' is undefined

library consist of a lib_XX.h file (for example )  & lib_XX.cpp file 

& like any other libraries i include .h file in main.c (my main program file )

#include ''lib_XX.h''

-----

libraries dosent have any problem & i used them in keil cpp project before.

is there any suggestion ?

best regards,Mary christmas

Mahmoud

3 REPLIES 3
tm3341
Associate II
Posted on December 27, 2014 at 15:36

C and C++ are not the same languages! You cannot combine them together.

''class'' word does not exists in C.

You have 2 options:

1. Convert your cpp file to C or

2. Do entire project in C++

mhdizgah
Associate II
Posted on December 28, 2014 at 10:23

actually im trying to convert my last project to cpp but there is a problem too:

im using

http://en.radzio.dxp.pl/ks0108/

to initial ks0108 GLCD with stm32f103 , every thing is ok except

GLCD_Bitmap

function

void GLCD_Bitmap( const unsigned char * bmp, unsigned char x, unsigned char y, unsigned char dx, unsigned char dy)
{
unsigned char i, j;
for(j = 0; j < dy / 8; j++)
{
GLCD_GoTo(x,y + j);
for(i = 0; i < dx; i++) 
GLCD_WriteData(GLCD_ReadByteFromROMMemory(bmp++));
}
}

it draws a stored image,

GLCD_WriteData

function dosent have any problem because other functions used it correctly.

this function declared on ks0c file

when there is not declaration of this function on ks0h (

void GLCD_Bitmap( const unsigned char * bmp, unsigned char x, unsigned char y, unsigned char dx, unsigned char dy);

) compiler show this warning but program run correct .

warning: #223-D: function ''GLCD_Bitmap'' declared implicitly

but when i add that declaration to ks0h it show error & dosent compile:

error: #167: argument of type ''const unsigned char (*)[1024]'' is incompatible with parameter of type ''const unsigned char *''

im completely mixed up,

i attached completed project if any one help me or give me a other example of ks0108 with stm32

----------------------------

http://www.edaboard.com/attachments/112673d1419752501-ks0zip

---

thanks for any help

--------------------------------

SOLVED

carl2399
Associate III
Posted on December 30, 2014 at 00:20

C and C++ combine very nicely - thank you very much.

I use this all day every day to migrate projects from C to a hybrid of C and C++ on the STM32.

The only requirements are:

1. To call C from C++ make sure you have extern ''C'' before the C function definition.

2. To call C++ from C, make sure you have extern ''C'' before the C++ function definition, and it has to be a simple function (i.e. not part of a class). I'll often do this to make interface functions into the C++ from C.

eg in C++

class Control_Class

{

public:

    int Status;

    void Task(void);

} Control;

extern ''C'' void Control_Task(void)

{

    Control.Task();

}

extern ''C'' int Control_Status(void)

{

    return Control.Task();

}

In this example, Control_Task and Control_Status are both able to be called from C.

In this way you can transition to C++ one source file at a time.

I can't really see any disadvantages to using C++, as long as you apply the following rules:

1) No new() and delete(). All classes static.

2) No run time type information.

3) No streams. (i.e. no << or >> operators for streaming to serial ports).

If you follow these rules, the size of your binary will not increase. In fact the majority of my projects shrink between 10% and 30% because of the improved structuring that's possible.

Rule 1 can be broken if you don't mind using malloc and free in your code.

Rule 3 can probably be broken without much penalty in the code, but I never have.

The nett result is that my C++ looks like structures with function calls. However you do gain inheritance and abstract classes / virtual functions. 

You don't have to make a 100% commitment to C++. Give it a try, you wont look back!