2020-09-26 12:57 PM
I'm using follow code:
volatile unsigned int *DWT_CYCCNT = (volatile unsigned int *)0xE0001004; //address of the register
volatile unsigned int *DWT_CONTROL = (volatile unsigned int *)0xE0001000; //address of the register
volatile unsigned int *DWT_LAR = (volatile unsigned int *)0xE0001FB0; //address of the register
volatile unsigned int *SCB_DEMCR = (volatile unsigned int *)0xE000EDFC; //address of the register
*SCB_DEMCR |= 0x01000000;
*DWT_LAR = 0xC5ACCE55; // unlock
*DWT_CYCCNT = 0; // reset the counter
*DWT_CONTROL |= 1 ; // enable the counter
uint32_t start=0, end=0;
uint32_t array[100];
uint32_t idx=0;
*DWT_CYCCNT = 0;
start = *DWT_CYCCNT;
idx=1;
end = *DWT_CYCCNT;
idx=0;I put a breackpoint on line 18 and I get:
start=9
end=22
*DWT_CYCCNT = 29
I'm expecting that start could be something like 2 and end something like 4 or 6. Why I get this results?
Is DWT working in an stm32f722?
thank
2020-09-26 1:20 PM
These are C statements, not assembly. Examine the disassembly to see what instructions are between start and end. Cache and flash wait states can also have an effect.
2020-09-27 9:10 AM
Time 100 or 1000 iterations of the code to benchmark, subtract out overhead of empty vs test loop
2020-09-28 7:12 AM
The problem I see is a difference between cortex M4 (stm32f411) and M7 (stm32f722)
On M4 I can run the code posted and I get exactly 2 cycle, I can run this other code:
*DWT_CYCCNT = 0;
uint_test=1; // 2 ciclos
*DWT_CYCCNT = 0;
float_test=1; // 2 ciclos
*DWT_CYCCNT = 0;
float_test=3.4f * 1.000054f;
*DWT_CYCCNT = 0;
float_test=3.4 * float_test;and get exactly what I expect on debug viewer.
But on M7 I get very wrong values.
I can't find on stm32f722 reference manual the implementation of DWT_CYCCNT. So I'm wondering about the working of this module on M7
In fact, DWT_CYCNT is changing ther values (counting) without code line 6 to 9 on first post. It seems like the DWT is configured and enabled by default? My project is generated using cubemx tool.
2020-09-28 7:23 AM
I'm very confused.
I create a new empty project using SystemWorkbench IDE. I don't include HAL library, just startup file.
Then create a main.c file and write:
volatile unsigned int *DWT_CYCCNT = (volatile unsigned int *)0xE0001004; //address of the register
volatile unsigned int *DWT_CONTROL = (volatile unsigned int *)0xE0001000; //address of the register
volatile unsigned int *DWT_LAR = (volatile unsigned int *)0xE0001FB0; //address of the register
volatile unsigned int *SCB_DEMCR = (volatile unsigned int *)0xE000EDFC; //address of the register
int main(void)
{
// *SCB_DEMCR |= 0x01000000;
// *DWT_LAR = 0xC5ACCE55; // unlock
// *DWT_CYCCNT = 0; // reset the counter
// *DWT_CONTROL |= 1 ; // enable the counter
int uint_test=0;
float float_test =0.0f;
float f1=3.14f, f2=3.15f;
*DWT_CYCCNT = 0;
uint_test=1; // 2 ciclos
*DWT_CYCCNT = 0;
float_test=1; // 2 ciclos
*DWT_CYCCNT = 0;
float_test=3.4f * 1.000054f;
*DWT_CYCCNT = 0;
float_test=3.4 * float_test;
*DWT_CYCCNT = 0;
float_test=f1 * f2;
*DWT_CYCCNT = 0;
}I get wrong values on expression viewer (debug and step by step) and get HardFault on line 26! what am I missing????
Same code on a fresh project running on stm32f411 (with lines 8..11 uncommented) get right values for DWT_CYCCNT but HardFault on line 26.