cancel
Showing results for 
Search instead for 
Did you mean: 

Driving TFT-LCD on STM32Fx with HAL

ehsan2754
Associate II
Posted on July 01, 2016 at 17:07

Hello guys,

I am using Keil Uvision 5.2 and cube Mx for developing STM32 MCUs.

and I want to Drive a TFT-LCD which the size is 2.8 inch and it has 320*240 pixels and it has ILI9328 driver inside.

I have few information about driving this LCDs such as it has different modes for driving such as 8-bit parallel driving, 16bit parallel driving and SPI mode.

and I found some libraries for driving this LCD but that is not clear to use and uses CMSIS drivers.

could anybody helpd  me optimizing this library for HAL and STM32Fx MCU and using FSMC.

I really need this library please.!!!!:D

thank you
1 REPLY 1
slimen
Senior
Posted on July 02, 2016 at 14:51

Hi,

It's better to create one thread for the same topic.

So, we can keep all answer in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Driving%20TFT-LCD%20on%20STM32Fx%20with%20HAL&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx&currentviews=7]thread.

Regards