Double buffered DMA Interrupt not working
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-02 1:01 AM
Posted on August 02, 2014 at 10:01
Hi All,
New to the STM32 so please bare with me.... I have setup timer4 to generate a sinewave modulated PWM using double buffered DMA and that works very well, I can see my waveform on the pin and it contains the correct data from each of the two buffers. However, I am trying to update the buffers via the half completed interrupt and I don't seem to be getting any action at all ... The code that sets up the DMA and the interrupt and the interrupt routine itself follows: ------------------------------------------------------------------- void DMA_Configuration(void) { DMA_InitTypeDef DMA_InitStruct; NVIC_InitTypeDef NVIC_InitStructure; // TIM4_UP - DMA1, Channel 2, Stream 6 DMA_InitStruct.DMA_Channel = DMA_Channel_2; DMA_InitStruct.DMA_BufferSize = PWM_ELEMENTS; DMA_InitStruct.DMA_DIR = DMA_DIR_MemoryToPeripheral; DMA_InitStruct.DMA_Mode = DMA_Mode_Circular; DMA_InitStruct.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStruct.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStruct.DMA_Memory0BaseAddr = (uint32_t)&PWM_Buffer[0]; DMA_InitStruct.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStruct.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStruct.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStruct.DMA_PeripheralBaseAddr = (uint32_t)&TIM4->CCR1; DMA_InitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStruct.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStruct.DMA_Priority = DMA_Priority_Medium; DMA_Init(DMA1_Stream6, &DMA_InitStruct); // Disable stream DMA_Cmd(DMA1_Stream6, DISABLE); // Configure double DMA mode. // This function can be called only when the DMA Stream is disabled. DMA_DoubleBufferModeConfig(DMA1_Stream6,(uint32_t)&PWM_Buffer2[0],DMA_Memory_0); // Enable DMA double mode. This function can be called only when the DMA Stream is disabled. DMA_DoubleBufferModeCmd(DMA1_Stream6, ENABLE); //!Enable DMA transfer complete interrupt DMA_ITConfig(DMA1_Stream6, DMA_IT_TC, ENABLE); NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream6_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_EnableIRQ(DMA1_Stream6_IRQn); // turning DMA on DMA_Cmd(DMA1_Stream6, ENABLE); } // Interrupt handler for dma transfer 1/2 finished, i.e after one buffer done. void DMA1_Stream6_IRQHandler(void) { // Stream6 transfer complete interrupt? if(DMA_GetITStatus(DMA1_Stream6, DMA_IT_TCIF6)) { // Transfer Complete event // clear pending interrupt DMA_ClearITPendingBit(DMA1_Stream6, DMA_IT_TCIF6); if(DMA_GetCurrentMemoryTarget(DMA1_Stream6)) { } else{ } } } ----------------------------------------------------------------- Can anyone help? EDIT: This is on a STM32F4Discovery Board
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-02 1:08 PM
Posted on August 02, 2014 at 22:08
Using a C++ compiler?
Does the handler show up in the .MAP file, and do you have linkage to it through the vector table?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-08-02 1:33 PM
Posted on August 02, 2014 at 22:33 Hi Clive, No it is not in the .map file, how do I link it for this processor? That name is in the vector table, I just thought you had to define it? Cheers, Bernie