2015-05-11 4:12 PM
So in `SD_PowerON` there is a comment at the bottom that says `/* else MMC Card */`. `hsd->CardType` is never set to `MULTIMEDIA_CARD` which is defined in `stm32f4xx_hal_sd.h`, and read in `HAL_SD_WideBusOperation_Config`. I have generated a project in the Cube and changed the `Mode` of `SDIO` to `eMMC 4 bits wide`, but it doesn't seem any different to the SD version. Here is the function for reference:- /**
* @brief Enquires cards about their operating voltage and configures clock
* controls and stores SD information that will be needed in future
* in the SD handle.
* @param hsd: SD handle
* @retval SD Card error state
*/
static HAL_SD_ErrorTypedef SD_PowerON(SD_HandleTypeDef *hsd)
{
SDIO_CmdInitTypeDef sdio_cmdinitstructure;
__IO HAL_SD_ErrorTypedef errorstate = SD_OK;
uint32_t response = 0, count = 0, validvoltage = 0;
uint32_t sdtype = SD_STD_CAPACITY;
/* Power ON Sequence -------------------------------------------------------*/
/* Disable SDIO Clock */
__HAL_SD_SDIO_DISABLE();
/* Set Power State to ON */
SDIO_PowerState_ON(hsd->Instance);
/* 1ms: required power up waiting time before starting the SD initialization
sequence */
HAL_Delay(1);
/* Enable SDIO Clock */
__HAL_SD_SDIO_ENABLE();
/* CMD0: GO_IDLE_STATE -----------------------------------------------------*/
/* No CMD response required */
sdio_cmdinitstructure.Argument = 0;
sdio_cmdinitstructure.CmdIndex = SD_CMD_GO_IDLE_STATE;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_NO;
sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
sdio_cmdinitstructure.CPSM = SDIO_CPSM_ENABLE;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdError(hsd);
if(errorstate != SD_OK)
{
/* CMD Response Timeout (wait for CMDSENT flag) */
return errorstate;
}
/* CMD8: SEND_IF_COND ------------------------------------------------------*/
/* Send CMD8 to verify SD card interface operating condition */
/* Argument: - [31:12]: Reserved (shall be set to '0')
- [11:8]: Supply Voltage (VHS) 0x1 (Range: 2.7-3.6 V)
- [7:0]: Check Pattern (recommended 0xAA) */
/* CMD Response: R7 */
sdio_cmdinitstructure.Argument = SD_CHECK_PATTERN;
sdio_cmdinitstructure.CmdIndex = SD_SDIO_SEND_IF_COND;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_SHORT;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp7Error(hsd);
if (errorstate == SD_OK)
{
/* SD Card 2.0 */
hsd->CardType = STD_CAPACITY_SD_CARD_V2_0;
sdtype = SD_HIGH_CAPACITY;
}
/* Send CMD55 */
sdio_cmdinitstructure.Argument = 0;
sdio_cmdinitstructure.CmdIndex = SD_CMD_APP_CMD;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
/* If errorstate is Command Timeout, it is a MMC card */
/* If errorstate is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch)
or SD card 1.x */
if(errorstate == SD_OK)
{
/* SD CARD */
/* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */
while((!validvoltage) && (count <
SD_MAX_VOLT_TRIAL
))
{
/* SEND CMD55 APP_CMD with RCA as 0 */
sdio_cmdinitstructure.Argument
=
0
;
sdio_cmdinitstructure.CmdIndex
=
SD_CMD_APP_CMD
;
sdio_cmdinitstructure.Response
=
SDIO_RESPONSE_SHORT
;
sdio_cmdinitstructure.WaitForInterrupt
=
SDIO_WAIT_NO
;
sdio_cmdinitstructure.CPSM
=
SDIO_CPSM_ENABLE
;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
if(errorstate != SD_OK)
{
return errorstate;
}
/* Send CMD41 */
sdio_cmdinitstructure.Argument = SD_VOLTAGE_WINDOW_SD | sdtype;
sdio_cmdinitstructure.CmdIndex = SD_CMD_SD_APP_OP_COND;
sdio_cmdinitstructure.Response = SDIO_RESPONSE_SHORT;
sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
sdio_cmdinitstructure.CPSM = SDIO_CPSM_ENABLE;
SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
/* Check for error conditions */
errorstate = SD_CmdResp3Error(hsd);
if(errorstate != SD_OK)
{
return errorstate;
}
/* Get command response */
response = SDIO_GetResponse(SDIO_RESP1);
/* Get operating voltage*/
validvoltage = (((response >> 31) == 1) ? 1 : 0);
count++;
}
if(count >= SD_MAX_VOLT_TRIAL)
{
errorstate = SD_INVALID_VOLTRANGE;
return errorstate;
}
if((response & SD_HIGH_CAPACITY) == SD_HIGH_CAPACITY) /* (response &= SD_HIGH_CAPACITY) */
{
hsd->CardType = HIGH_CAPACITY_SD_CARD;
}
} /* else MMC Card */
return errorstate;
}
Note: this post was migrated and contained many threaded conversations, some content may be missing.
2018-05-21 10:52 AM
For me DMA is the ultimate and only goal
:)
.2018-05-21 11:01 AM
Using DMA here (polling is too fragile), clocking SDIO peripheral from 100 MHz SYSCLK (F412 allows this), bus clock at 50 MHz and 4-bit mode for eMMC
Here with 32KB block sizes, writing same 32MB file second time was a tad slower, probably erase costs.
32768000 Bytes, 240338076 Cycles
13.63 MBps Write (FatFs) 2403 ms run time 13.64 MBps (Sanity Check)32768000 Bytes, 253318235 Cycles
12.94 MBps Write (FatFs) 2533 ms run time 12.94 MBps (Sanity Check)32768000 Bytes, 166638903 Cycles
19.66 MBps Read (FatFs) 1666 ms 19.67 MBps SysTick Sanity32768000 Bytes, 166645439 Cycles 19.66 MBps Read (FatFs) 1667 ms 19.66 MBps SysTick Sanity2018-05-21 11:08 AM
>>I founds that the non-DMA versions of those functions are unreliable and produce FIFO underrun errors as other people have reported on this forum.
Agreed, polled is very fragile/marginal, issues with interrupts, and contention from LTDC, etc. Always use DMA here, so haven't seen often, but stock examples for F7-DISCO boards have been observed to be marginal and tend to fail when stressed slightly. Typically building on additional code. Problems more visible on DSI when pixel clocks pushed 30-60 MHz
2018-05-21 11:12 AM
I tried to get DMA to work on the F7, but the error flags would trigger randomly and thereseemed to be no way to tell if the error was real or not. The H7 may be better.
I also upgraded the FatFS version to get its more recent features
2018-12-27 2:36 AM
did u find any solution for eMMC support.can give me some suggestion to proceed .iam trying to interface eMMC stm32l4r9i eval board
2018-12-27 2:36 AM
did u find any solution for eMMC support.can give me some suggestion to proceed .iam trying to interface eMMC stm32l4r9i eval board
2018-12-27 2:37 AM
did u find any solution for eMMC support.can give me some suggestion to proceed .iam trying to interface eMMC stm32l4r9i eval board.iam afraid to say that u have attached orginal cubemx generated file not the one which supports emmc,can you please share the file again?
2018-12-27 3:47 PM
The ODROID method proposed by Nemui has been applied successfully to a number of L4 and L4+ NUCLEO and DISCO boards. Waiting on delivery of an STM32L4R9I-EVAL, and expect that to be workable also.