2013-12-26 6:00 PM
Hi,
I'm posting for the first time here. Does STM32L100RC have opamps? I'm asking this because I am finding conflicting information: When I go to: http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1295 and click on ''2'' and ''3'' under ''Integrated op-amps'', STM32L100RC shows up. When I click on STM32L100RC in the product selector above, I am taken to the product page, which does not mention op amps under ''Analog peripherals''. When I download the PDF datasheet (not the reference manual), the list of features on the first page of the datasheet does not mention op amps either. However, when I look at the pin descriptions in the same datasheet, I do find OPAMP1_VINP and its friends mentioned. I'm confused. If somebody could clarify this, that would be greatly appreciated. Thanks,2013-12-26 6:32 PM
See the Reference Manual Section 14.
Cheers, Hal2013-12-27 10:56 AM
Baird,
Thank you for a quick response. I guess the device does have opamps because Section 14 of the reference manual starts out with: ''This section applies to high and medium+ density devices only.'' http://www.st.com/st-web-ui/active/en/catalog/mmc/FM141/SC1169/SS1295/LN1808/PF255680 starts out with: ''The medium density plus ultra-low-power STM32L100RC incorporates ...''2013-12-27 11:31 AM
The Datasheet /
Reference Manual are the definitive documents - product selectors, etc, just give a ''first pass'' overview to allow you to narrow-down a reasonably small set of possible candidates.
Also, the front page of a datasheet is just a ''headline'' summary - you need to study the full text to get the full picture.http://www.8052.com/forum/read/190215