cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32H743 mcu support ONFI1.0?

IRyu.1
Associate

I am going to use STM32H743 mcu.

And I am trying to configure the nand-flash memory test circuit using this chip (using the EVL board).

What I want to ask is whether you can use nand-flash memory chip that supports only ONFI1.0 as STM32H743 chip.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

NAND might be better achieved via eMMC, 8-bit and DDR modes being supported by the SDMMC interface.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I'm not sure what specific aspects of ONFi you are looking to use. The FMC (External Bus) on the H7 is rather agnostic to the hardware interface specifics, and has a finite set of pins to implement memory banks/selects. If you need additional signals perhaps look at how you can use address bus bits to drive them, and then use offsets within the decode window to actuate those signals high/low.

Any query methods on the array/geometry would need to be implemented in user's driver code.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..