cancel
Showing results for 
Search instead for 
Did you mean: 

Does not create a project in CUBEMX for stm32f411

valik mahrov
Associate II
Posted on May 08, 2018 at 19:54

HI.I recently bought myself a board with a STM32f411 nucleo. And there was a problem in the fact that CUBEMX hovered and did not close it. What should I do? Thank you in advance!

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
Nesrine M_O
Lead II
Posted on May 09, 2018 at 11:21

Hi

valik250403

,

there was a problem in the fact that CUBEMX hovered and did not close it

  • What is the

    CUBEMX version are you using?

  • Do you mean that you are not able to open CUBEMX?

    Maybe you shouldclean your cache and try again

  • Could you please give more details about your issue?

-Nesrine-

valik mahrov
Associate II
Posted on May 09, 2018 at 11:37

I'm using version 4.24.0. And the thing is when I open the project and start generating the code for STM32F411RE, my CUBEMX hangs. When I select another STM32 everything works normal without freezes.

Posted on May 09, 2018 at 11:44

Hi

valik250403

,

Could you please try to use the last CUBEMX version (4.25) and tell us if the issue still again.

-Nesrine-

valik mahrov
Associate II
Posted on May 09, 2018 at 16:35

Same.

Nesrine M_O
Lead II
Posted on May 09, 2018 at 16:38

Hi

valik250403

,

This is reported to our MX team for check!

-Nesrine-

valik mahrov
Associate II
Posted on May 09, 2018 at 16:40

Good. I'm waiting.

Nawres GHARBI
ST Employee
Posted on May 10, 2018 at 12:32

Hi

valik250403

Could you please attach the ioc, it will help for debug

valik mahrov
Associate II
Posted on May 11, 2018 at 11:24

Using your ioc the project is well generated and compiled correctly, it seems that there is an issue related to your install or PC. 

Could you please put the log file of CubeMX in a comment, you will find it under  /user_folder/.stm32cubemx/STM32CubeMX.log