2011-07-26 12:30 AM
Hi,
unfortunately somehow all attachements of older posts seem to have gone. Does anybody of you still have the code from Relaxe? That he posted in the thread/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/SDIO %2b FAT16FAT32&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B
Best Tom null2011-07-26 01:02 AM
2011-07-26 01:51 AM
Thanks for the pointer. I just read the document and it only states
There is freeware in the file system on the web and some are licensed versions availablefrom companies. I downoaded the firmware package and the FAT lib is only included as object file, no source and I'm pretty sure that it's no open source. Best Tom
2011-07-26 02:22 AM
you can use free file system like EFSL or FAT_FS-ELM. these are freely available in the web.
________________ Attachments : STM32_mini_dpf_pub_20091128.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Gg&d=%2Fa%2F0X0000000bkW%2FdYDpuuZjVenEUD3QWYWgJ6hw2Q5C_vltCur3rcLBaKA&asPdf=false2011-07-26 02:33 AM
I forgot to mention. In the last post I attached an example source code in which FAT_FS is used.
2011-07-26 03:28 AM
Thanks, I already had one implementation with Elm Chan FAT.
Relaxe did it with DosFS. I would like to compare this one with Elm Chans version. Best Tom