2007-12-20 9:52 AM
DMA USART1 problem
2011-05-17 3:20 AM
I have run into a frustrating problem and would welcome any suggestions/insight. I have a high frequency interrupt from timer3 invoking an IRQHandler at about 100KHz (system clock is 64MHz). I also have USART1 set up for DMA on DMA channels 4 and 5. The USART is setup for full duplex RS-232 at 115200 baud. I have a host side program sending a 5 byte command over the USART. The main loop of the program replies with a 5 byte reply packet out the USART.
Here's the problem. If the TIM3 IRQHandler writes to any peripheral on APB2, it cause the DMA channel 4 (USART1_TX) to skip a byte every now and then - that is, it sends 4 bytes instead of 5. the DMA_CNDTR4 is always set to 5 and is never interfered with directly in any way during the transmission. APB2 HCLK is set to highest speed. The TIM3 IRQHandler can do just about any thing else - write to APB1 peripherals, read and write to RAM, do large time consuming math operations, etc. without compromising the USART1_TX DMA, but as soon as you throw in a write to any APB2 peripheral - GPIOx, SPI1, ADC1, etc - it starts causing the occasional dropped byte. It doesn't seem that I am violating duty cycle limitations on the APB2 bus but perhaps I'm missing something?2011-05-17 3:20 AM
Dear fpmartin,
You can refer to our App Note AN2548 :'' Using the STM32F101xx and STM32F103xx DMA controller'' this may help you to design your system while using DMA with other peripherals. let us know if you need further details Regards, STOne-32