cancel
Showing results for 
Search instead for 
Did you mean: 

DMA question

kornfeldner
Associate II
Posted on June 24, 2009 at 05:05

DMA question

1 REPLY 1
kornfeldner
Associate II
Posted on May 17, 2011 at 13:15

Is it possible to setup two DMA channels with one DMA controller, that starts automatically the next channel when first channel is finished ?

i tried it out but the two channels are always alternating.

the first channel has higher priority than the second channel but no success.

is there a solution ?